Skip to main content
nooshin_1382
Associate III
Aug 25, 2015 7:44 AM UTC
Question

Problem With LINFLEX1 Interrupt

Posted on August 25, 2015 at 09:44

Hi

In my system i set the LINFLEX1 For my Lin Connections I set this in Master Mode i send and recive correctlly the slave response but i don't have any interrupt on Vector99 what is the problem on SPCstudio ??

Thanks For Help

Best Regards

Nazerian Vanima
    This topic has been closed for replies.

    4 replies

    Erwan YVIN
    ST Technical Moderator
    Aug 25, 2015 1:05 PM UTC
    Posted on August 25, 2015 at 15:05

    Hello Vanima ,

    Did you set this following register during configuration mode ?

    linflexp->LINIER.R = SPC5_LINIER_DTIE | SPC5_LINIER_DRIE |
    SPC5_LINIER_BOIE | SPC5_LINIER_FEIE |
    SPC5_LINIER_SZIE; 
    /* Interrupts enabled. */

    if you do not use UART / LINFLEX1 .. you should unplug from your SPC5Studio configuration. Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    nooshin_1382
    Associate III
    Aug 26, 2015 7:22 AM UTC
    Posted on August 26, 2015 at 09:22

    Hi Erwan

    Thanks For Your Response

    My Problem is not solved , i enabled these before but have no response in interrupt.

    I have a slave sensor when i send a wake up id for sensor the sensor recive the data successfully when i want to recive a data from slave node i put the id on bus (Refer to ReciveData in my code on attachment ) i recive the response , i check the data on UDE Debugger it is correct but i have not any interrupt .

    i send my code on attachment if code have any problem tell me about .

    thanks so much.

    Best Regards

    Nazerian Vanima

    ________________

    Attachments :

    main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qa40&d=%2Fa%2F0X0000000bpB%2FuqvrFL19z7jj1mSmc4s7t_9f7BG74GiyzRzsosXnO7g&asPdf=false
    Erwan YVIN
    ST Technical Moderator
    Aug 28, 2015 9:29 AM UTC
    Posted on August 28, 2015 at 11:29

    Hello Vanima ,

    I have forwarded your point to your LINFLEX Experts in AUTOSAR Team.

                 Best Regards

                            Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    ST Technical Moderator
    Aug 28, 2015 1:40 PM UTC
    Posted on August 28, 2015 at 15:40

    Hello Vanima ,

    Your LINFLEX configuration seems to be good and the timeout is disable.

    Could you check your CPR configuration ?

    The INTC_CPR masks any peripheral or software configurable interrupt request set at the same or lower priority as the current value of the INTC_CPR[PRI] field from generating an interrupt request to the processor.

    Best regards

                                  Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.