Skip to main content
HCast
Visitor II
Apr 30, 2019 3:27 PM UTC
Question

Problem with BAFusing CAN and SPC5 connect

Hello,

I am trying to initialize BAF on microcontroller SPC5 using SPC5 connect and SPC5 flash programmer. When I try to connect it I get the following error:

[2019/04/30 10:12:19]: SPC5 Flash Programmer 2.7.1 - Start connection: Target:SPC58EC70 - External crystal: 16MHz - Interface: UCCAN::SPC5Connect/0/CAN

[2019/04/30 10:12:22]: An error occured during plugin downloading via BAM/BAF

[2019/04/30 10:12:22]: Connection end.

I monitored the communication channel and got the following results:

0690X000008B7bYQAS.png

It seems the device is sending the password several times. I also checked the microcontroller registers and in the PSR[LEC] register from CAN Channel I got a value refering to BIT0 error code.

Does anybody know what the problem is? How can I solve it?

Thanks!!!

    This topic has been closed for replies.