Skip to main content
Vitaliy Anzin
Associate
Aug 27, 2018 10:02 AM UTC
Question

Problem with ADC on the Bernina

Hello,

I've got a problem with max analog channel input voltage. When all supply voltages are 5V everything is fine. But if VDD_HV_IO_MAIN voltage is 3.3V while VDD_HV_ADV is 5V, the analog channel input voltage becomes limited over 4V. This problem is observed both on my PCB and on the EVB (SPC57xxMB + SPC58XXADPT176S REV. B). Can you help me resolve the problem?

    This topic has been closed for replies.

    1 reply

    Vitaliy Anzin
    Associate
    Aug 28, 2018 7:17 AM UTC

    More test results for the problem: MCU temperature increases for 6-7 degrees. It seems the analog channel internal circuit scheme protection is referenced by VDD_HV_IO_MAIN (instead VDD_HV_ADV). Сan someone clarify this?