Skip to main content
prashanth.mohan22
Associate III
Jun 3, 2019 7:34 AM UTC
Question

Problem in sending continuous stream of data in UART

Hi,

Please find the piece of code, where i'm transmitting a buffer of 255 bytes of data.

int main(void) {
	uint8_t read[255];
	uint16_t size;
	for(i=0;i<255;i++)
	{
		read[i]=i+1;
	}
	size = sizeof(read)/sizeof(read[0]);
 
	componentsInit();
 
	irqIsrEnable();
 
	sd_lld_start(&SD2, &serial_config_cfg1);
 
	if(sd_lld_write(&SD2,read,size) == SERIAL_MSG_OK)
	{
	 pal_lld_setpad(PORT_C, PC_LED7);
	 osalThreadDelayMilliseconds(200);
	}
return 0;
}

My output looks like this. Lot of data are being missed on UART Transmission.

01
02
03
04
05
06
07
08
09
0a
0b
0c
0d
0e
0f
10
11
12
13
14
15
16
17
18
19
1a
1b
1c
1d
1e
1f
20
21
22
23
24
25
26
27
28
29
2a
2b
2c
2d
2e
2f
30
31
32
33
34
35
36
37
38
39
3a
3b
3c
3d
3e
3f
40
41
42
4c
64
7c
88
91
9b
a4
ae
b7
c0
ca
d3
dc
e7
f0
fa

After 0x42, I'm not receiving continuous stream of data, and much of the data are being missed in vain. Help me in debugging it.

Note:

  1. I have checked by transmitting uint32_t type data. Large portion of data is being skipped in this case as well.
  2. while debugging step by step, the tx interrupts are occurring correctly and I could retrieve without missing any data.

Thanks for your help in advance.

Prashanth Mohan

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Jun 28, 2019 9:28 AM UTC

    Hello ,

    Did you solve your issue ?

    Have you tried to increase the stack size ?

    Which device do you use ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    prashanth.mohan22
    Associate III
    Jun 28, 2019 10:02 AM UTC

    Hi Erwan,

    Yes the issue is solved, the problem is the system clock of the other end is slower than the transmitting clock, I used a little bit delay before transmission of each byte and now I could retrieve the data safely.

    Thanks.

    Prashanth Mohan