Skip to main content
prashanth.mohan22
Associate III
May 28, 2019 12:47 PM UTC
Solved

Problem in connecting to the target SPC560Bxx Disc board

0690X000008a5MpQAI.png

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 28, 2019 1:48 PM UTC

    Hello , Could you check your device manager ?

    You should see PLS USB JTAG

    0690X000009XiaZQAS.png

    if not , install the drivers located in

    c:\Program Files (x86)\pls\UDE 4.10\Driver\

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 28, 2019 1:48 PM UTC

    Hello , Could you check your device manager ?

    You should see PLS USB JTAG

    0690X000009XiaZQAS.png

    if not , install the drivers located in

    c:\Program Files (x86)\pls\UDE 4.10\Driver\

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    prashanth.mohan22
    Associate III
    Jul 15, 2019 7:22 AM UTC

    Hi @Erwan YVIN​ ,

    I've connected the device to my PC. The lights are glowing on the board, but the PC is not detecting it as USB and hence no COM ports are assigned to it. Is it a problem with the SPC560B-DIS hardware?

    My other SPC560B-DIS board is working fine. Help me resolve this issue.

    Regards,

    Prashanth