Skip to main content
Central SUPPORT
Senior
Jun 3, 2019 3:45 PM UTC
Solved

PIT timer of SPC560P50L5 to be used for wake up

We use SPC560P50L5 in an automotive-qualified battery management system for starter batteries. PIT timer of this device should be able to generate a wake-up interrupt when in low-power mode.

At this moment, PIT timer 3 is already working to generate an interrupt at the end of a certain time period. The user manual states that it is possible to use the PIT timer to leave low-power mode (STOP0). But it is unclear which registers are used for that, and how we have to configure them. 

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

    This topic has been closed for replies.
    Central SUPPORT
    Central SUPPORTBest answer
    Senior
    Jun 3, 2019 3:46 PM UTC

    For PIT to be used for wake-up it needs some additional settings, so let me summarize following three main points:

    1.     CLK has to be enabled for PIT, but since PIT3 is already working I suppose that this point is done

    -      Register PITMCR_MDIS

    2.    Interrupt has to be enabled and you have to clear the flag after an interrupt has occured.

    -      Register TCTRL3 for enable

    -      Register TFLG3_TIF for clearing flag

    3.    Configure the STOP0 mode to keep the PIT enabled and working

    -      ME_STOP0_MC for configuration of used mode, important is that SYSCLK is running.

    -      ME_LP_PC0_STOP0 should be enabled.

    -      ME_PCTL92_LP_CFG should be set to “000�?, which selects ME_LP_PC0 configuration.

    1 reply

    Central SUPPORT
    Central SUPPORTAuthorBest answer
    Senior
    Jun 3, 2019 3:46 PM UTC

    For PIT to be used for wake-up it needs some additional settings, so let me summarize following three main points:

    1.     CLK has to be enabled for PIT, but since PIT3 is already working I suppose that this point is done

    -      Register PITMCR_MDIS

    2.    Interrupt has to be enabled and you have to clear the flag after an interrupt has occured.

    -      Register TCTRL3 for enable

    -      Register TFLG3_TIF for clearing flag

    3.    Configure the STOP0 mode to keep the PIT enabled and working

    -      ME_STOP0_MC for configuration of used mode, important is that SYSCLK is running.

    -      ME_LP_PC0_STOP0 should be enabled.

    -      ME_PCTL92_LP_CFG should be set to “000�?, which selects ME_LP_PC0 configuration.