Skip to main content
zhu.chang-qing
Associate
Jun 17, 2015 6:40 AM UTC
Question

osal sleep

Posted on June 17, 2015 at 08:40

Hello,

I am a newer of SPC studio, while I am learning SPCstudio,

I read help docs such as ''SPC560Pxx OS-less OSAL Component User Manual.chm''

I don't understand how this function ''osalThreadSleepMilliseconds(1000);'' implement ,even though I go into it for details.

Does anyone know how this function works? It sleeps for a while ,then wake up,or it use a system timer (STM)  to delay some time.

Thanks!

#spcstudio
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Jun 17, 2015 8:26 AM UTC
    Posted on June 17, 2015 at 10:26 Hello Zhu ,

    osalThreadSleepMilliseconds(1000); is based system tick calculated from the PIT Channel 0

    (Periodic Interrupt Timer) (cf below)

    /**
    * @brief PIT channel 0 interrupt handler.
    *
    * @isr
    */
    OSAL_IRQ_HANDLER(vector59) {
    OSAL_IRQ_PROLOGUE();
    osalSysLockFromISR();
    osalOsTimerHandlerI();
    osalSysUnlockFromISR();
    /* Resets the PIT channel 0 IRQ flag.*/
    PIT.CH[0].TFLG.R = 1;
    OSAL_IRQ_EPILOGUE();
    }

    Initilialization is done in hal_lld_init()

    /* PIT channel 0 initialization for Kernel ticks, the PIT is configured
    to run in DRUN,RUN0...RUN3 and HALT0 modes, the clock is gated in other
    modes.*/
    INTC.PSR[59].R = SPC5_PIT0_IRQ_PRIORITY;
    halSPCSetPeripheralClockMode(92,
    SPC5_ME_PCTL_RUN(2) | SPC5_ME_PCTL_LP(2));
    reg = halSPCGetSystemClock() / OSAL_ST_FREQUENCY - 1;
    PIT.PITMCR.R = 1;

    /* PIT clock enabled, stop while debugging. */

    PIT.CH[0].LDVAL.R = reg;
    PIT.CH[0].CVAL.R = reg;
    PIT.CH[0].TFLG.R = 1;

    /* Interrupt flag cleared. */

    PIT.CH[0].TCTRL.R = 3;

    /* Timer active, interrupt enabled. */
    Best Regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    zhu.chang-qing
    Associate
    Jun 18, 2015 3:53 AM UTC
    Posted on June 18, 2015 at 05:53

    hi, erwan!

    Thank you so much!

    I will go trough it.