Skip to main content
Santhamurthy R
Associate III
May 24, 2017 9:33 AM UTC
Question

Nonvolatile Registers in SPC560B54L5

Posted on May 24, 2017 at 11:33

Hello All,

I am working on SPC560B54L5 board using SPC5studio version 5.2.3

In my bootloader application i have to do some operations depends on the flag set by Main application

i don't want to use the EEPROM or Flash to do this,

Is there any Register,where I can try to read the data written by Main application  in bootloader application as it is after resetting the MCU.

Someone please let me know,  is there any CPU register which will retrieve the data in it even after the system reset.

Thanks in Advance,

With Regards,

R.Santhamurthy

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Jun 14, 2017 8:12 AM UTC
    Posted on June 14, 2017 at 10:12

    Hello R.Santhamurthy ,

    There is No Non-Volatile Register in SPC560B54L5

    You should use the DFLASH.

       Best regards

                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.