Skip to main content
Yalin Gurcan
Associate III
Jun 5, 2018 8:58 AM UTC
Question

No COM Port seen in Win7 on SPC570S-DISP

Posted on June 05, 2018 at 10:58

Hi all, I've got a SPC570S-DISP eval board and I've been trying to get the sample serial code working. The LED's are working fine and I'm sure rest of the code is fine too but I cannot see any COM Ports in device manager. I've installed FTDI and VCP drivers but it still is not showing. I can see the JTAG adapters in USB controllers, for reference. Does anybody else have this problem? Thanks in advance.

#com #usb-virtual-port-com-(vcp) #spc570s-disp
This topic has been closed for replies.

3 replies

Erwan YVIN
ST Technical Moderator
Jun 6, 2018 8:26 AM UTC
Posted on June 06, 2018 at 10:26

Hello Yalin ,

You should set ''Load VCP'' in Drivers Settings (PLS USB JTAG Adapeter for SPC5xxx A

 0690X0000060L8cQAE.png

Best regards

         Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Yalin Gurcan
Associate III
Jun 6, 2018 11:03 AM UTC
Posted on June 06, 2018 at 11:03

Hello Erwan,

I have managed to see the PLS USB Serial Port in device manager but I'm only seeing one port whereas I should have 2, one for JTAG/programming stuff and the other one for LINFLEX0, am I right? I cannot connect to COM4 while UDE is loaded with the workspace.0690X0000060L8SQAU.png

Erwan YVIN
ST Technical Moderator
Jun 7, 2018 9:29 AM UTC
Posted on June 07, 2018 at 09:29

Hello Yalin ,

You have to choose the good COM port

1 is for the debugging

1 is for the LINFLEX (38400 Bauds COM20 is my example)

0690X0000060LAsQAM.png

      Best regards

                    Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.