Skip to main content
Msert.1
Associate II
Nov 11, 2020 8:34 PM UTC
Solved

Multi-Core Questions

Hi,

It is a SPC56EC Dual core sample project which comes with SPCStudio (I imported the project form your library) and I have some questions. The screenshot is attached.

1- When we use dual core at the same time, how do they memory sharing? They share same memory or not?

2- We enable the core_0 with the runCore(); statement and program goes to "int main_core0(void)" function. My question is how program knows to must go there. main_core0 is a uniqe identifier or I can give a name it randomly?

3- Have setting done in sample project about for relating peripherals and cores? For example, when I initialize ADC module in Low Level Driver Comp., for using core 0 or core1; I just should add module's functions in related function ( I mean for using ADC module in Core_0 then I should add main_core0 function).

Stay safe,

Best Regards

0693W000005B5zpQAC.png

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Nov 13, 2020 3:33 PM UTC

    I assume you are referring to SPC58EC example.

    1) Multicore example delivered with SPC5Studio memory is shared across the two cores.

    2) main_core0 is a symbol that is used crt0.s file. See this file to understand how main_core0 symbol is used.

    3) Yes your understanding is correct: any function called by main_core0() will be executed on Core_0. Any function called by main() will be executed by Core_2

    Regards,

    Giuseppe

    2 replies

    Giuseppe DI-GIORE
    ST Employee
    Nov 13, 2020 3:33 PM UTC

    I assume you are referring to SPC58EC example.

    1) Multicore example delivered with SPC5Studio memory is shared across the two cores.

    2) main_core0 is a symbol that is used crt0.s file. See this file to understand how main_core0 symbol is used.

    3) Yes your understanding is correct: any function called by main_core0() will be executed on Core_0. Any function called by main() will be executed by Core_2

    Regards,

    Giuseppe

    Msert.1
    Msert.1Author
    Associate II
    Nov 16, 2020 6:20 AM UTC

    Thanks a lot Giuseppe!

    Best Regards,