Skip to main content
May 16, 2019 7:41 AM UTC
Solved

Motor Control 1.1.0 installation Problem

I try to install the SPC5-MCTK-LIB_RTM_1_1_0_web under SPC5Studio 5.8.1 according to the "Quick Start Guide Motor Control ToolKit for SPC5Studio". First I Updated the whole IDE and added the available components. Then I tried to install the MCTK-LIB.

When I reach the Steps described at Page 14 (Add local Software), I see how the IDE tries to compute alternate solutions while clicking next, where I get the following Error:

"Cannot complete the install because one or more required items could not be found.

 Software being installed: SPC56xx Web Motor Control Feature 1.0.0.201807231455 (com.st.spc5.components.spc5rla.spc56xx.webmotorcontrol.feature.feature.group 1.0.0.201807231455)

 Missing requirement: SPC56xx Web Motor Control Feature 1.0.0.201807231455 (com.st.spc5.components.spc5rla.spc56xx.webmotorcontrol.feature.feature.group 1.0.0.201807231455) requires 'com.st.spc5.components.spc5rla.spc5xx.full.feature.feature.group 1.5.0' but it could not be found"

Is it possible to get the MotorControl-Kit 1.1.0 working under SPC5Studio 5.8.1?

And, if yes, what am I doing wrong?

Best regards,

Adrian

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Feb 10, 2020 3:56 PM UTC

    Dear All ,

    in SPC5Studio 5.8.1 :

    For the MCTK backward compatibility for SPC5Studio 5.8.1

    1)  you should add : (Cloudforge is down)

    http://mirrors.spc5studio.com/rla-mctk

    2)   And Install the current version of MCTK

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    5 replies

    May 16, 2019 9:39 AM UTC

    LIKE :smiling_face_with_heart_eyes: --> the Error dissappeared and the installation is working again, seems like I need to learn more about legacy-problems, but the MCTK (1.1 is the actual Version) seems to be installed, so thanks from Germany

    ABota
    Visitor II
    Sep 2, 2019 1:02 PM UTC

    Hello,

    I had the same issue and fixed it with your help, but there's another problem when trying to build the project (Regardless which of the Web Motor Control Demos I choose).

    The steps I made are:

    1.) Import samples from application

    2.) Choose one of the motor control applications

    3.) Generate the SPC5 Application

    4.) Build the SPC5 Application

    The last step generates following error message:

    ./components/spc56xx_web_motor_control_component/lib/System_Drive_Params/src/Spc5xxx_MC_it.c:48:21: fatal error: pal_lld.h: No such file or directory

     #include "pal_lld.h"

    Which is a bit strange, since I didn't make any changes to the configuration.

    Can you please help?

    a-daniel
    Visitor II
    Jan 22, 2020 10:08 AM UTC

    Hi,

    Did you find any solutions to this issue ?

    I have the same error with SPC5-MCTK-LIB 1.1.0 and SPC5Studio 5.8.1 .

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Feb 10, 2020 3:56 PM UTC

    Dear All ,

    in SPC5Studio 5.8.1 :

    For the MCTK backward compatibility for SPC5Studio 5.8.1

    1)  you should add : (Cloudforge is down)

    http://mirrors.spc5studio.com/rla-mctk

    2)   And Install the current version of MCTK

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    TJ Oen
    Visitor II
    Sep 8, 2020 8:43 AM UTC

    I have the same problem using SPC5 studio 6.0. http://mirrors.spc5studio.com/rla-mctk not working.