Skip to main content
souha
Associate
Jun 1, 2015 3:08 PM UTC
Question

LIN use in spc560b60L3

Posted on June 01, 2015 at 17:08

Hello

I am using the spc560B60L3 100 pin package. For my application , I need to use 4 LINflex interfaces.

In the data sheet, it is mentioned that it supports 4 LINs.Can we use LIN4 and LIN5 or it only supports LIN0 up to LIN3?

Regards,
    This topic has been closed for replies.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    Jun 2, 2015 1:42 PM UTC
    Posted on June 02, 2015 at 15:42

    Hello Souha ,

    Yes , you can use LIN4 and LIN5 on LQFP100

    To configure it ,

    you have to set the PADSEL associated Table

    cf screenshot on Pinmap Wizard

    Best regards

    Erwan

    ________________

    Attachments :

    2015-06-02_154111.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWct&d=%2Fa%2F0X0000000boR%2FhkrWYt4GfM1H5pOo8NwFGewvS7aMv1.dBP7oh_UiKRA&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    souha
    souhaAuthor
    Associate
    Jun 2, 2015 2:59 PM UTC
    Posted on June 02, 2015 at 16:59

    Hello Erwan,

    Thanks  for your response. Can I use LIN5 and LIN4 in serial mode? IN spc5studio when I activate this function it generates an error saying that it is not supported in spc560B60L3.

    Regards,

    Erwan YVIN
    ST Technical Moderator
    Jun 5, 2015 7:57 AM UTC
    Posted on June 05, 2015 at 09:57

    Hello Souha ,

    You are right ;) There is a bug in SPC56BXX HAL Drivers you can update the file spc560b_registry.h to solve the issue :

    #elif defined(_SPC560B60L3_)
    #define SPC5_NUM_DSPI 3
    #define SPC5_NUM_LINFLEX 6
    #define SPC5_NUM_GPIO 77

    We have submitted an error report for HAL drivers. it will be corrected asap on the official update site. Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    souha
    souhaAuthor
    Associate
    Jun 10, 2015 2:18 PM UTC
    Posted on June 10, 2015 at 16:18

    Hello Erwan,

     

    By this update,only avoid errors in spc5 studio when LIN4 or LIN5 is activated. But it cannot be used as SCI. I tried to start serial communicaton (sdStart(&SD5,NULL)) after enabling linflex4 in serial mode, the code crashes. This is not the case when I use LIN0 up to LIN3.

    Erwan YVIN
    ST Technical Moderator
    Jun 10, 2015 3:14 PM UTC
    Posted on June 10, 2015 at 17:14 Hello Souha , There is a bug in spc5_linflex.h (SPC5-HAL) you should have :

    #if SPC5_HAS_LINFLEX4 || defined(__DOXYGEN__)
    #define SPC5_LINFLEX4 (*(struct spc5_linflex *)0xFFE50000UL)
    #endif

    it corrects the DATA ABORT. we will correct it in the next version of SPC5-HAL. Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.