Skip to main content
Subham Roy_O
Visitor II
Jun 16, 2017 6:05 AM UTC
Solved

License check for trace stream failed for SPC560P50L5

Posted on June 16, 2017 at 08:05

I am working on a CAN bus based project on the SPC560P50L5 platform. The project is based on the CAN RLA example included with the SPC5Studio.

Details about my setup:

  1. SPC5Studio version 5.3
  2. UDE debug kit version 4.02.07 (SPC-UDESTK-EVAL license)
  3. SPC5-UDESTK JTAG debugger (

    http://www.st.com/resource/en/data_brief/spc5-udestk.pdf

     )
  4. GNU FreeGCC compiler with VLE

My project code size is way less than the UDE debugger EVAL license limit (i.e. 256kB). The size of my project code is as follows:

text    data    bss    dec    hex filename

11630      0   2128  13758   35be build/out.elf

When I try to flash the program with UDE debugger I get this error

Fr 16.06.2017 11:17:21.586, Error, MCUManager, License check for trace stream 'Controller0_NexusTrace' error: no valid license for UDE trace add-on found

Fr 16.06.2017 11:17:21.586, Error, MCUManager, Trace stream object 'Controller0_NexusTrace' was removed to due missing license key features

 

I have tested by using both the external debugger module (SPC5-UDESTK) and the on-board debugger, but in both cases the above error was shown and I couldn't flash the program.

I can confirm that there is no problem with the UDE debugger installation, as I have one another SPC560D40L1 board and UDE is able to flash and debug it just fine.

Is there a way to get around this problem?

Thanks!!

#spc #ude
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 16, 2017 7:17 AM UTC
    Posted on June 16, 2017 at 09:17

    Hello Subham ,

    you can find the starter kit keys in this following link :

    https://www.pls-mc.com/download-spc5-udestk/downloads-a-1626.html

     

    For your information, it is better to use 

    UDE debug kit version

    4.08.xx

        Best Regards

                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 16, 2017 7:17 AM UTC
    Posted on June 16, 2017 at 09:17

    Hello Subham ,

    you can find the starter kit keys in this following link :

    https://www.pls-mc.com/download-spc5-udestk/downloads-a-1626.html

     

    For your information, it is better to use 

    UDE debug kit version

    4.08.xx

        Best Regards

                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Matthias Noack
    Visitor II
    Aug 9, 2017 8:20 PM UTC
    Posted on August 09, 2017 at 22:20

    Hello,

    SPC5-UDESTK does not allow to do NEXUS trace. Therefore These warnings are output. If you like to get or use NEXUS trace please contact PLS directly:

    http://www.pls-mc.com