Skip to main content
ssk
Associate III
Jan 7, 2016 10:18 AM UTC
Question

Library files

Posted on January 07, 2016 at 11:18

I want to generate library files for my C modules. E.g. I have a C module for timer with functions for initialization, configuration, start and stop. I want to generate a library module which I can use in SPC5Studio project and call the required API from other C modules. Is it possible with SPC5Studio?

Can I build C module to generate library files?

Thanks.

Mike
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Jan 7, 2016 3:12 PM UTC
    Posted on January 07, 2016 at 16:12

    Hello Mike ,

    You should create an alternate project for this :

    Script and Makefile

    1) generate your .o files by an other makefile

    2) ppc-free-vle-ar ruv yourlib.a *.o 

       or ppc-cle-ar ruv yourlib.a *.o 

    In your application :

    3) Update user.mak file

    # Define ASM defines here

    UADEFS      =

    # List all user directories here

    UINCDIR     =

    # List the user directory to look for the libraries here

    ULIBDIR     =

    # List all user libraries here

    ULIBS       =

       Best regards

                      Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ssk
    sskAuthor
    Associate III
    Jan 15, 2016 9:43 AM UTC
    Posted on January 15, 2016 at 10:43

    Thanks Erwan. I shall look into building the library files.

    Best Regards,

    Mike