L9963 Evaluation Board with GUI does not work
- 5 replies
- 3177 views
Hello!
I performed the steps in manual to get it started. I could assign an ID and I could get the green ACK.
As soon as I try to go to the next step (3.2) configuring voltages the ACK turns red. Meaning I can´t send any configs to the device. I tried to read instead of writing, same outcome.
Sometimes I can get the ACK green again if I start diagnostic, sometimes I need to powercycle.
I connected the minimum pack voltage ( 2 cables) and I also tried the 4 cell connection with resistors- same outcome.
Open wire detection tells me only the first and the last cell are connected (after that the ACK for that button also turns red)
The attached AN states it should be Firmware 1.6...is there a new firmware? I have 1.5 (as the picture in the AN also shows) I can+t find any manual showing how to update the firmware.
What am I missing?