Skip to main content
270284440
Associate II
Apr 4, 2018 4:45 AM UTC
Question

K2 GTM tom0 driver issue based on Studio 5.7.2

Posted on April 04, 2018 at 06:45

I tested K2 GTM tom0 channel based on studio version 5.7.2.

for example ,tom0 ch0 output 20khz,50% ouput on io port selected in pin  -> it is OK,

if I configure tom0_ch0,ch1,ch2,ch3 with same frequence and duty ,and output to IOs,

then I did not see any pulse on IO ports.

but if I only enable one tom0 channel ,it is fine. is it bug in stuido?

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Apr 4, 2018 7:30 AM UTC
    Posted on April 04, 2018 at 09:30

    Hello Chu ,

    i am checking with experts.

               Best regards

                             Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    ST Technical Moderator
    Apr 9, 2018 10:53 AM UTC
    Posted on April 09, 2018 at 10:53

    Hello Chu ,

    Ticket has been submitted on GTM part

               Best regards

                      Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.