Skip to main content
stefanodimascio9
Associate III
Feb 26, 2016 8:53 AM UTC
Question

IVOR1 handling

Posted on February 26, 2016 at 09:53

Hello,

I have read the core manual of SPC56EL70 (e200z4). I want to handle the IVOR1 exception with an interrupt routine in configuration.xml in SPC5Studio. It's not clear to me what I should write in the ISR in question (what number? IVOR1 is not present in INTC chapter in the reference manual)

Thank you very much
    This topic has been closed for replies.

    4 replies

    Erwan YVIN
    ST Technical Moderator
    Feb 26, 2016 9:55 AM UTC
    Posted on February 26, 2016 at 10:55

    Hello Stefano ,

    Are you talking about Machine Check Interrupt (IVOR1)

    or ivor1 about the software vector table ?

            /* Software vectors table. The vectors are accessed from the IVOR4

               handler only. In order to declare an interrupt handler just create

               a function withe the same name of a vector, the symbol will

               override the weak symbol declared here.*/

    Already done in OSAL components

    1) for IVOR1,  (Machine Check Interrupt)

    you should update ivor.s (using patch mode)

    cf chapter 5.7.2 in e200z4RM.pdf

    http://cache.nxp.com/files/32bit/doc/ref_manual/e200z4RM.pdf?fpsp=1&WT_TYPE=Reference%20Manuals&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&fileExt=.pdf

    2) for ivor1 (software vector table) (from IVOR4)

    did you check Table 473. Interrupt sources for INTC_0 and INTC_1 ?

    in RM0342 , it is present.

    you should enable by OSAL component

       Best regards

                Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    stefanodimascio9
    Associate III
    Feb 26, 2016 10:18 AM UTC
    Posted on February 26, 2016 at 11:18

    I'm talking about the first one.

    So:

    I can just write an assembly routine, and I have to add at some point (I don't know exactly) of ivor.s:

    #if CORE_SUPPORTS_DECREMENTER

            /*

             * _IVOR1

             */

            .align      4

            .globl      _IVOR1

            .type       _IVOR1, @function

    _IVOR1:

            /* Creation of the external stack frame (extctx structure).*/

            stwu        %sp, -80(%sp)           /* Size of the extctx structure.*/

    #if PPC_USE_VLE && CORE_SUPPORTS_VLE_MULTI

            e_stmvsrrw  8(%sp)                  /* Saves PC, MSR.               */

            e_stmvsprw  16(%sp)                 /* Saves CR, LR, CTR, XER.      */

            e_stmvgprw  32(%sp)                 /* Saves GPR0, GPR3...GPR12.    */

    #else /* !(PPC_USE_VLE && CORE_SUPPORTS_VLE_MULTI) */

            stw         %r0, 32(%sp)            /* Saves GPR0.                  */

            mfSRR0      %r0

            stw         %r0, 8(%sp)             /* Saves PC.                    */

            mfSRR1      %r0

            stw         %r0, 12(%sp)            /* Saves MSR.                   */

            mfCR        %r0

            stw         %r0, 16(%sp)            /* Saves CR.                    */

            mfLR        %r0

            stw         %r0, 20(%sp)            /* Saves LR.                    */

            mfCTR       %r0

            stw         %r0, 24(%sp)            /* Saves CTR.                   */

            mfXER       %r0

            stw         %r0, 28(%sp)            /* Saves XER.                   */

            stw         %r3, 36(%sp)            /* Saves GPR3...GPR12.          */

            stw         %r4, 40(%sp)

            stw         %r5, 44(%sp)

            stw         %r6, 48(%sp)

            stw         %r7, 52(%sp)

            stw         %r8, 56(%sp)

            stw         %r9, 60(%sp)

            stw         %r10, 64(%sp)

            stw         %r11, 68(%sp)

            stw         %r12, 72(%sp)

    #endif /* !(PPC_USE_VLE && CORE_SUPPORTS_VLE_MULTI) */

    /*routine execution */

            b           _ivor_exit

    #endif /* CORE_SUPPORTS_DECREMENTER */

    Do I miss something?

    Erwan YVIN
    ST Technical Moderator
    Mar 1, 2016 1:28 PM UTC
    Posted on March 01, 2016 at 14:28

    Hello Stefano ,

    i think that it should be ok.

    What is your way to generate IVOR1 ?

      Best regards

                Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    stefanodimascio9
    Associate III
    Mar 1, 2016 1:49 PM UTC
    Posted on March 01, 2016 at 14:49

    That's something I'm struggling with: I need it in order to handle uncorrectable errors. I must disable ECSM reporting because I don't want a reset on DED in my application, but I don't have any mechanism to inject a DED avoiding reset: even if I enable ECSM reporting just for the injection, as the error is injected with

    SPP_MCM.EEGR.R= 0x0220;       //uncomment these three lines to inject uncorrectable error

      0x00014008:   70 1F E7 F4  E_LIS     R0,0xFFF4

      0x0001400C:   70 E0 02 20  E_LI      R7,0x220

      0x00014010:   01 06        SE_MR     R6,R0

      0x00014012:   5C E6 00 4A  E_STH     R7,0x4A(R6)

    *((uint32_t *) 0x40002000) = PATTERN;

      0x00014016:   62 10        SE_BGENI  R0,0x1         

      0x00014018:   65 20        SE_BSETI  R0,0x12

      0x0001401A:   70 EA E5 55  E_LIS     R7,0x5555

      0x0001401E:   70 EA C5 55  E_OR2I    R7,0x5555

      0x00014022:   01 06        SE_MR     R6,R0

      0x00014024:   D0 76        SE_STW    R7,0x0(R6)

    SPP_MCM.EEGR.R= 0x0000;

      0x00014026:   70 1F E7 F4  E_LIS     R0,0xFFF4

      0x0001402A:   48 07        SE_LI     R7,0x0

      0x0001402C:   01 06        SE_MR     R6,R0

      0x0001402E:   5C E6 00 4A  E_STH     R7,0x4A(R6)

    I have a  reset on the execution of: 0x00014016:   62 10        SE_BGENI  R0,0x1         

    This is not the behavior I expect, as on the manual is written that ECC is calculated on writings and checked at readings.