Skip to main content
Visitor II
May 6, 2026 9:42 AM UTC
Question

Is it impossible for the microcontroller to enter STANDBY0 when a debugger is connected?

My code is as follows.

 
volatile uint8_t d_deadcode = 0U;

void sleepManagement(void)
{
 if ((isIgnActive(IGN_1, getGpioInput(GPIO_IN_IGN_1))) ||
 (isIgnActive(IGN_2, getGpioInput(GPIO_IN_IGN_2))))
 {
		return;	/* ign sig exist */
	}

 if (isSleepSync())
 {
 sleepEntryHandler();
 d_deadcode = 1U;
 }
 else
 {
 	updateDateOld();
		requestSleepSync();
 }
}

static void sleepEntryHandler(void)
{
 uint32_t rtcWakeup;

 irqIsrDisable();
 deinitApp();

 if (ignOff1hrElapsed.state == OFF)
 {
 rtcWakeup = TIME_IGN_OFF_LOAD_60MIN - ignOff1hrElapsed.onTimer;
 startRtc(rtcWakeup);
 }

 startWkpu();
 enterStandby0();
}

void enterStandby0(void)
{
 /* 
 * PD0(8KB): always retained, not programmable
 * PD1(32KB): always lost in STANDBY0, not programmable
 * PD2(56KB): retain in STANDBY0
 */
 MC_PCU.PCONF2.B.STBY0 = ON;

 if (SPCSetRunMode(SPC5_RUNMODE_STANDBY0) == CLOCK_FAILED)
 {
 SPC5_CLOCK_FAILURE_HOOK();
 }
}​

I expected that when the device enters sleep mode and is woken up by the WKPU, a reset would occur and the crt0 routine would execute.

In reality, when I wake the device without a debugger connected and attach the T32 to check the d_deadcode value, it is 0.

However, when the device is woken up with the T32 connected, a breakpoint can be set at the line d_deadcode = 1U;, and an unintended hard fault occurs, causing it to fall into IVOR.

Does the debugger connection interfere with the device's low-power mode transition?