Skip to main content
ivancolla9
Associate III
Jan 27, 2016 10:32 AM UTC
Question

Inaccessible registers from source or with sfr

Posted on January 27, 2016 at 11:32

Good morning,

working with the universal debbuger on the dicscovery board with SPC56EL60L3, I have this error: various registers seem inaccesible to me. If I try to monitor them with SFR, I don't see the values, but ''???????'', and if I try to do an operation on one of them (reading or writing), the micro go in exception.

Modules that behave like this are, for example, CRC, ADC, LINFLEX.

For the ADC module I tried various configurations with the wizard, but nothing. 

I cannot understand why the ude cannot see them.

P. S: I reported the problem in the discussion on the STM register, because I thincked it was related to a single module (CRC), but after various trials it seems a generic problem related to a group of modules that, for some reason, I cannot access.

Thank you,

Ivan

#ude-sfr-registers-access
    This topic has been closed for replies.

    4 replies

    Erwan YVIN
    ST Technical Moderator
    Jan 27, 2016 1:43 PM UTC
    Posted on January 27, 2016 at 14:43

    Hello Ivan ,

    you have enable some IPs by associated PCTL (cf in RM) (cf memory map to have the associated number)

    /* clock gating if present.*/
    SPCSetPeripheralClockMode(?????,
    SPC5_ME_PCTL_RUN(2) | SPC5_ME_PCTL_LP(2));

    Best regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    ivancolla9
    Associate III
    Jan 28, 2016 2:43 PM UTC
    Posted on January 28, 2016 at 15:43

    Hello Erwan,

    thanks for the advice. I tried your solution, but it didn't work out. I cannot understand where to find that you suggested. If I copy the function name in my project (where I generated the board code with the wizard), I cannot find the function. Following the advice has been helpful. I discovered the ME module and the fact that peripherals must be activated. I found that the device, in RUN mode, had the peripherals deactivated, as you told. I used this code:

    /* Activate extern peripherals. */
    UBYTE ME_MASK = 0b11111111;
    ME.RUN_PC0.R = ME.RUN_PC0.R | ME_MASK;

    and it works. Do you have any suggestions regarding this piece of code? Any idea on why I cannot apply your solution? Probably I misinterpreted it. Thank you, Ivan
    ivancolla9
    Associate III
    Jan 29, 2016 10:35 AM UTC
    Posted on January 29, 2016 at 11:35

    I post here to add that the solution that I found have a strange problem.

    If I run the code step by step using the debugger, after the code that I posted I can use the ADC0 register.

    But in run mode, after the activation code, the register remains in ????? status and I go in exception.

    It seems that I miss something important.

    Someone have ideas?

    Thanks,

    Ivan

    Edit:

    I understood where the problem was. I missed this two lines (sorry for the bit notation):

    ME.MCTL.R = 0b01000000000000000101101011110000;

    ME.MCTL.R = 0b01000000000000001010010100001111;

    With this, I control a transition to the RUN0 state and configuration is loaded (so ADC converter is activated). First write: mode selection + key. Second write: mode selection + inverted key. See RM for Mode Control Register (ME_MCTL).

    The problem didn't arise when I was debugging, beacuse stopping the execution on a break point commanded automaticcaly a transition from DRUN to RUN0 mode loading the config.

    But if I didn't stop the application, the status of the system remained in DRUN and so my configuration were not loaded.

    Regards,

    Ivan

    Erwan YVIN
    ST Technical Moderator
    Feb 1, 2016 8:40 AM UTC
    Posted on February 01, 2016 at 09:40

    Hello Ivan ,

    Good that you find your issue ..

    not easy to find , but often the solution is in the RM;-)

      Best regards

                 Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.