Skip to main content
PE.1
Visitor II
Dec 14, 2020 9:41 AM UTC
Solved

In UDE VP, I cant able to flash the elf file as the core(SPC560p) toggles between inactive and running. Can anyone help me to sort out this issue. If it is a source code issue then anyone pls suggest me how to rectify this issue. Thanks in advance.

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Jan 11, 2021 8:26 PM UTC

    Hello,

    configure the UDE debugger to connect to the device at BAM address (that is just after the reset).

    It should be able to get the device back to flash-able state.

    See the UDE debugger help for further details (target configuration).

    Regards,

    Giuseppe

    1 reply

    Giuseppe DI-GIORE
    ST Employee
    Jan 11, 2021 8:26 PM UTC

    Hello,

    configure the UDE debugger to connect to the device at BAM address (that is just after the reset).

    It should be able to get the device back to flash-able state.

    See the UDE debugger help for further details (target configuration).

    Regards,

    Giuseppe