Skip to main content
CCOLL.2
Associate II
September 15, 2022
Solved

If I use SPC5 studio, do I need to be on a STM discovery kip or evaluation board to be able to flash and debug a board with a SPC582B or SPC584B MCU (I have also a probe SPC5-UDESTK) ?

Hi,

I'm new in SPC5 world.

I would like to use SPC5-Studio to start my project on a SPC582B product and I would like to be able to debug it.

I have a probe SPC5-UDESTK that I have used to flash a project compiled with SPC5-Studio.

It is not clear if I need to by some licences or if I can continue with free licence.

I have also read that the debug purposes of SPC5-studio is only available on STM development kits. Is-it the case ?

Do I need to use PLS UDE STK tool to debug a project or, is-it possible using SPC5-studio directly ? do I need to buy a new licence in order to debug ?

Thanks,

Christophe

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    September 16, 2022

    Hello,

    for SPC582B-DIS , (Discovery Kit)

    https://www.st.com/en/evaluation-tools/spc582b-dis.html

    you do need SPC5-UDESTK just a USB Mini cable is enough to flash and debug

    for SPC582B (Motherboard and Mini-Module)

    you need SPC5-UDESTK and USB Mini cable

    It includes a perpetual, full-feature, limited code-size (256 kBytes) license. (Flash and debug)

    it is often enough for projects

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    5 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    September 16, 2022

    Hello,

    for SPC582B-DIS , (Discovery Kit)

    https://www.st.com/en/evaluation-tools/spc582b-dis.html

    you do need SPC5-UDESTK just a USB Mini cable is enough to flash and debug

    for SPC582B (Motherboard and Mini-Module)

    you need SPC5-UDESTK and USB Mini cable

    It includes a perpetual, full-feature, limited code-size (256 kBytes) license. (Flash and debug)

    it is often enough for projects

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    CCOLL.2
    CCOLL.2Author
    Associate II
    September 16, 2022

    Hi,

    Thanks for your answer.

    But, if I do not use a STM board (I have a prototype done by a customer), is SPC5 studio able to debug on it ?

    We plan to make a new project based on the same SPC582B or 4B chip and I would like to use this board to work on it during the pre-study.

    Rgds,

    Christophe

    Erwan YVIN
    ST Technical Moderator
    September 16, 2022

    Hello Christophe ,

    I hope that the JTAG port is well present and well plugged in your prototype board.

    SPC5-UDESTK could be plugged.

    Anyway , SPC5 Studio is eclipse based.

    It is possible to install to additional plugins (TRACE32,PLS UDE or others compliant for PPC VLE e200z) , debug and flash.

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    CCOLL.2
    CCOLL.2Author
    Associate II
    September 16, 2022

    Hi,

    Yes, on the previous project, JTAG was used to flash the board only so, I assume that it is physicaly OK.

    Thanks for the info about plugins, I have just installed the UDE plugin.

    I will check how many signals are available in the JTAG interface but, as we have already a trace32 probe (even if I suppose that we need a specific interface for SPC5), it could be interresting to use it during this pre-study.

    Rgds,

    Christophe

    jmary
    Associate III
    September 17, 2022

    Hi, I create spc5-udestk from the SPC574 discovery board schematic.

    Anyone willing to send me the ude memtool flash programmer?