Skip to main content
orhanyilmaz
Associate III
Dec 1, 2014 11:38 AM UTC
Question

I2C Peripheral Control

Posted on December 01, 2014 at 12:38

Hello,

I trying use the I2C periph. But, It is not work. Have you a I2C referance manual ? or What should I do? My Example code :

void
I2C_initial(
void
)
{
/*
* Note: Clk is startup enabled.
* for Ex:
* ME.RUNPC[1].R = 0x00000010;//.B.RUN0 = 1;//
*
* ME.PCTL[44].R = 0x01; //I2C0 - RunPC[1]
* //Mode Transition to Enter RUN0 MODE
* ME.MCTL.R = (0x40000000|KEY);//RUN0 MODE & KEY
* ME.MCTL.R = (0x40000000|INVERT_KEY);//RUN0 MODE
*
* //Check Configurations
* while(ME.GS.B.MTRANS);//Global Status Register wait for mode transition to complete
*
* while(ME.GS.B.CURRENTMODE != 4);//Global Status Register verify RUN0 Current mode
*
*/
////////////////////////////////////////////////////////////////
// I2C Pads
////////////////////////////////////////////////////////////////
//CLK
//SIU.PCR[PA11].R = 0x0800; //I2C SCL
SIU.PCR[PB3].R = 0x0800; 
//I2C SCL
//DATA
//SIU.PCR[PA10].R = 0x0800; //I2C SDA
SIU.PCR[PB2].R = 0x0800; 
//I2C SDA
//SDA Select
//SIU.PSMI[30].B.PADSEL = 0; //for PA10
SIU.PSMI[30].B.PADSEL = 1; 
//for PB2
////////////////////////////////////////////////////////////////
////////////////////////////////////////////////////////////////
I2C_0.IBAD.B.ADR = 0x02;
//Address = 0x01
/*
* IBC7-6 - MUL
* -------------
* 00 -> 1
* 01 -> 2
* 10 -> 4
* 11-Reserved
*
* IBC5-3 scl2start scl2stop scl2tap tap2tap
* ---------------------------------------------------------
* 000 2 7 4 1
* 001 2 7 4 2
* 010 2 9 6 4
* 011 6 9 6 8
* 100 14 17 14 16
* 101 30 33 30 32
* 110 62 65 62 64
* 111 126 129 126 128
*
* IBC2-0 SCL_Tap SDA_Tap
* ------------------------------------
* 000 5 1
* 001 6 1
* 010 7 2
* 011 8 2
* 100 9 3
* 101 10 3
* 110 12 4
* 111 15 4
*
* RM0017 pdf(page 355-357) for more
*/
I2C_0.IBFD.B.IBC = 0;
I2C_0.IBCR.B.MDIS = 0; 
//Module Enable
I2C_0.IBCR.B.IBIE = 0; 
//Bus Interrupt Disabled
I2C_0.IBCR.B.MS = 1; 
//Master mode
I2C_0.IBCR.B.RSTA = 1; 
//Generate repeat start cycle
////////
}
//
void
I2C_Write(U_8 data)
{
I2C_0.IBSR.B.IBIF = 1;
//Flag Clear
I2C_0.IBCR.B.MS = 1; 
//Master mode
I2C_0.IBCR.B.TX = 1;
I2C_0.IBDR.B.DATA = data; 
//( Page: 360 )
I2C_0.IBCR.B.RSTA = 1;
}

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Dec 3, 2014 2:23 PM UTC
    Posted on December 03, 2014 at 15:23

    Hello Yilmaz ,

    Your code seems to be correct

    To enable I2C, it is mandatory to set the peripheral clock mode.

    if not , it will generate a reset issue when you try to write to the volatile memory I2C_0

    cf example below for B512K

    /* Sets peripheral clock.*/

      halSPCSetPeripheralClockMode(44, SPC5_ME_PCTL_RUN(1) | SPC5_ME_PCTL_LP(2));

    do not forget to handle the interruptions

    OSAL_IRQ_HANDLER(vectorXX)

    you have an I2C example in chapter 20.5.1 of RM017

      Best regards

                Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.