Skip to main content
Sk1
Visitor II
Jan 29, 2020 5:13 AM UTC
Question

I wanted to know JTAG PIN details of the SPC5-UDESTK-PLUS Debugger

Hi All,

I am unable to connect target to the UDE.

1)Is there any necessity to install virtual Com port drivers for debugging with UDE-STK-PLUS debugger apart from the drivers provided by the UDE software ?

2) How to integrate SPC5 studio with UDE-STK-PLUS ?

3) Also, please share  JTAG PIN details of the SPC5-UDESTK-PLUS Debugger. So that I can verify the target connection with UDE-STK-PLUS.

Thanks in advance.

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Jan 30, 2020 9:32 AM UTC

    Hello Sk ,

    1) No, Virtual Com Port drivers are only useful to use Serial Port (using printf mecanism)

    2) There are "UDE Eclipse 4 integration" in http://spc5tools.spc5studio.com/

    you can install it

    but PLS UDE should be installed in your PC

    3) Which board do you use ? i think that the information is in the datasheet

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.