Skip to main content
guo qiang
Senior
Jun 26, 2017 9:46 AM UTC
Solved

i have two SPC5 I2C Driver problem and The SPC5studio IDE problem

Posted on June 26, 2017 at 11:46

question 1:

i2c_result_t i2c_lld_write(uint8_t dev_addr, uint16_t reg_addr,uint8_t *data, uint8_t ndata_bytes)

{

..................

  /* Check for valid address */

   if ((dev_addr < 8U) || (dev_addr > 119U))

   {

      return I2C_ERROR_INVALID_ADDRESS;

    }

................

}

Why is the slave address between 8-119? Is this slave address 7bit or 8bit?

question 2:

My project uses FreeRTOS, each time the code generated, the macro configUSE_TIMERS will automatically become 0. And the Makefile in the compiler parameters will automatically become -O2. Each modification is very troublesome, how can I do?

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 26, 2017 2:31 PM UTC
    Posted on June 26, 2017 at 16:31

    Hello ,

    Question 1:

    Why is the slave address between 8-119?Is this slave address 7bit or 8bit?

    A seven bit wide address space theoretically allows 128 I2C addresses – however, some addresses are reserved for special purposes. Thus, only 112 addresses are available with the 7 bit address scheme

    Question 2:

    the Makefile is generated

    1) -O2 is set in the platform component

    2) for the timer , Go to SPC5 FreeRTOS Component RLA and check Use Software timers

    ==> Save and generate

    Best regards

    Erwan

    ________________

    Attachments :

    2017-06-26 16_29_21-workspace - SPC5Studio - SPC560Dxx_RLA FreeRTOS SERIAL Test Application for Disc.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyaO&d=%2Fa%2F0X0000000b9p%2FcQTNlN6H2MIIhv4R2XkT0FZrTS8nW6Vzy2iacPUnNDQ&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    5 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 26, 2017 2:31 PM UTC
    Posted on June 26, 2017 at 16:31

    Hello ,

    Question 1:

    Why is the slave address between 8-119?Is this slave address 7bit or 8bit?

    A seven bit wide address space theoretically allows 128 I2C addresses – however, some addresses are reserved for special purposes. Thus, only 112 addresses are available with the 7 bit address scheme

    Question 2:

    the Makefile is generated

    1) -O2 is set in the platform component

    2) for the timer , Go to SPC5 FreeRTOS Component RLA and check Use Software timers

    ==> Save and generate

    Best regards

    Erwan

    ________________

    Attachments :

    2017-06-26 16_29_21-workspace - SPC5Studio - SPC560Dxx_RLA FreeRTOS SERIAL Test Application for Disc.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyaO&d=%2Fa%2F0X0000000b9p%2FcQTNlN6H2MIIhv4R2XkT0FZrTS8nW6Vzy2iacPUnNDQ&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    guo qiang
    guo qiangAuthor
    Senior
    Jun 27, 2017 2:45 AM UTC
    Posted on June 27, 2017 at 02:45

    0690X00000607WIQAY.png

    ....Why i did not........

    0690X00000607H4QAI.png

    SPC5 Studio, version: 5.4

    Erwan YVIN
    ST Technical Moderator
    Jun 27, 2017 9:05 AM UTC
    Posted on June 27, 2017 at 09:05

    Hello Guo ,

    You have not clicked on the good configuration settings.

    0690X00000607WSQAY.png

    Click on the outline view to change your panel (cf SPC5Studio Help)

           Best regards

                  Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.