Skip to main content
Jkoya
Associate
Oct 9, 2019 4:40 AM UTC
Question

I am using SPC5b6054 microcontroller. I am trying to develop LIN driver. It is working properly ,but i need to change delimiter length. I did't find the register in data sheet to change it. Please suggest me a way to change the delimiter length.

..

    This topic has been closed for replies.

    5 replies

    prashanth.mohan22
    Associate III
    Oct 14, 2019 8:58 AM UTC

    hi @Erwan YVIN​ ,

    Can you please help on this one.

    By default we are getting one bit for delimiter. But as per the LIN Descriptor File, delimiter should hold two bits. Kindly let us know a way to change the delimiter length, as we couldn't find the appropriate register in the datasheet.

    Best Regards,

    Prashanth Mohan

    Erwan YVIN
    ST Technical Moderator
    Oct 16, 2019 1:57 PM UTC

    Hello ,

    I think that it is located in BIDR register0690X00000AqR65QAF.png

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    prashanth.mohan22
    Associate III
    Oct 16, 2019 2:19 PM UTC

    Hi Erwan,

    Thanks for your response, but unfortunately, what we are asking is not about Data Field Length which is number of data bytes in the RESPONSE part of the frame.

    But we are asking about the delimiter bit length in the SYNC Brake Field of header part of the frame.

    PFA,

    0690X00000AqR8aQAF.png

    While connecting to LIN channel to the analyzer, we are getting on is "sync delimiter error". In our chip, we could able to select the break length in MBL register field of LINCR1 register, but not the delimiter length.

    0690X00000AqRDGQA3.png

    Currently we are setting MBL as 18 bits and by default it is taking the delimiter length as 1 bit, upon which, we are getting "delimiter bit error" in LIN Analyzer.

    Please help us on this.

    Best Regards,

    Prashanth Mohan

    Erwan YVIN
    ST Technical Moderator
    Oct 16, 2019 2:43 PM UTC

    I think that it is not configurable and it should be 1 Bit

    About the error

    "This Error bit bit is set by hardware when the delimiter is too short (in other words, less than one bit time).

    It should be cleared by software."

    I have checked in All families SPC56,SPC57 and SPC58 .. No configuration is possible on Delimiter bit length

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Jkoya
    JkoyaAuthor
    Associate
    Oct 17, 2019 2:07 PM UTC

    0690X00000AqUqQQAV.png0690X00000AqUrJQAV.png0690X00000AqUquQAF.pngHi Erwan ,

    Thanks for your reply.

    SPC_LIN_waveform_9600BPS(first image) screen shot is the LIN wave form generated by SPC microcontroller, which is captured in oscilloscope.

    According to this waveform, the delimiter length is not less than one bit, But still i am getting the same error which i mentioned in CANanalyse_LIN(second image) screen shot.

    Actual required wave form is mentioned in Simulated_master_node(third image) screen shot.