Skip to main content
RRama.8
Associate II
Jan 22, 2020 2:44 PM UTC
Solved

I am currently working on Chorus 10M context swapping functionality. I am trying to flash two software in two different banks but I am unable to do that. I am trying to flash with the help of Debugger. But I couldn't do that. Thanks in advance.

I am able to switch between the banks. But writing a software in the banks is failure one.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 28, 2020 3:23 PM UTC

    Hello Rama ,

    i think that you should update the linker file (application.ld)

    Did you use SPC5 Studio ?

    Which debugger do you use ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jan 28, 2020 3:23 PM UTC

    Hello Rama ,

    i think that you should update the linker file (application.ld)

    Did you use SPC5 Studio ?

    Which debugger do you use ?

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    RRama.8
    RRama.8Author
    Associate II
    Jan 29, 2020 8:28 AM UTC

    Hello Erwan,

    Thanks for coming back. I am using SPC5 Studio only and i am isystems debugger. I tried changing the Linker script(application.ld) even though there is no use. Any leads will help me