Skip to main content
RSeba.2
Associate III
Jan 26, 2023 1:05 PM UTC
Question

I am configuring the flexray controller.After setting the parameters, a RUN command is given which changes the POC_state from POC:ready to POC:startup. But further change of state to POC:normalactive is not observed.

The FlexRay cluster I have here consist of 2 FlexRay cold-start nodes and the third node, spc58ec mcu non-cold start node. Can anybody suggest what can go wrong ?

This topic has been closed for replies.

4 replies

JLi.311
Associate
Feb 8, 2023 6:57 AM UTC

I also want to use the FlexRay, Is this code write by yourself or transplant from other project?

Erwan YVIN
ST Technical Moderator
Feb 23, 2023 4:15 PM UTC

Hello Sebastian ,

Have you solved your issue ?

it could be due to the loss of synchronization with the network.

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
RSeba.2
RSeba.2Author
Associate III
Feb 24, 2023 9:39 AM UTC

Hello,

Currently I am doing the transmit buffer configurations. I configured 2 transmit buffers. But the FLEXRAY_0.CH[1].MBIDXR.B.MBIDX field is still 0 even after setting an index. Do you know why is it so ?

Kind regards,

RSeba

RSeba.2
RSeba.2Author
Associate III
Feb 24, 2023 5:02 AM UTC

Hello,

Yes. It has been resolved. The issue was with the MCR register's configuration. After correctly setting the MCR register, I reached the expected protocol state normal active.

Thanks and kind regards,

RSeba