Skip to main content
NUndi.1
Visitor II
May 3, 2021 2:12 PM UTC
Solved

How to write my manufacturer device configuration Data on Customer OTP region in case of SPC582b60e MCU.

Hi,

I am using SPC584b60e MCU, I have to write several hundred byte of data at Customer OTP region which is there in first block flash memory. I am not getting how I can start. I have following question

1) Can I use C55 flash module API to write at this region, if so how I can start, because I don't see any example for writing at OTP region in SPC5 studio ?

2) Can I write data here word by word (32-bit at a time ) instead of whole block write ?

3) What is sequence to initialize, unlock and write at this customer OTP location.

Please provide if any example code is available

Thank you

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 2, 2021 1:39 PM UTC

    Hello Nundi ,

    you can use C55 flash module API in order to write in One-Time Programmable (OTP) area Test Flash Block

    for thers questions, i recommend to go in the RM0449 for additional questions.

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 2, 2021 1:39 PM UTC

    Hello Nundi ,

    you can use C55 flash module API in order to write in One-Time Programmable (OTP) area Test Flash Block

    for thers questions, i recommend to go in the RM0449 for additional questions.

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.