Skip to main content
FCui
Visitor II
Nov 5, 2019 6:38 AM UTC
Question

How to use processor core local RAM of the MCU SPC584C70E3?

Dear

I noticed there are 64K core local RAM in the MCU SPC584C70E3. Does this area is used exclusively by the processor core? Can it be used as general SRAM by user code? If can, how to use it? 

Thanks!

    This topic has been closed for replies.

    1 reply

    Angelo Castello
    ST Employee
    Feb 12, 2021 3:56 PM UTC

    Good morning,

    You are right. The device has 64KiB per Core's of local RAM memory mapped and accessible by means of :

    0x50800000 0x5080FFFF D-MEM CPU_0

    0x52800000 0x5280FFFF D-MEM CPU_2

    For your device part number SPC584C70E3 you have only a single Core then only one Local RAM @ 0x52800000

    One typical use case is something like this :

    char myVar[32] __attribute__ ((section (".dmemcpu2"))) = { ...

    You need only to add the section dmemcpu2 into your linker script.

    Hoping to meet your request.

    Regards,

    Angelo