Skip to main content
Rajesh_
Associate
Sep 11, 2019 9:12 AM UTC
Question

how to set SPC560b50l3 to STOP mode?

I am able to set STOP mode in SPC560B50l3 successfully, but still the total

current drawn is 6-7mA.

According to datasheet the maximum current consumed in stop mode under 55 °C is 500 uA.

Following is the code that i have added to set STOP mode:

ME.STOP0.B.PDO=1;/* Pad power sequence driver disabled, but state */

                     /* of the output is kept */

   ME.STOP0.B.MVRON=0;   /* Main Voltage regulator is off */

   ME.STOP0.B.DFLAON=1;  /* Data flash is in power-down mode */

   ME.STOP0.B.CFLAON=1;/* Code flash is in power-down mode */

   ME.STOP0.B.FXOSC0ON =0;/* Fast external crystal oscillator (4-16 MHz) off */

   ME.STOP0.B.FMPLLON =0;/* FMPLL is off (default status during STOP0) */

   ME.STOP0.B.SYSCLK=0xf; /* System clock disabled BEFORE RC switching off */

   ME.STOP0.B.FIRCON =0;/* Fast internal RC oscillator (16 MHz) off */

   ADC.MCR.B.PWDN = 1; /* Power donw analog part of ADC0 */

   ME.MCTL.R = 0xA0005AF0;   //request STOP mode

   ME.MCTL.R = 0xA000A50F;   //request STOP mode

   while(ME.GS.B.S_MTRANS);

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Sep 17, 2019 12:41 PM UTC

    Hello ,

    I forward your point to the good guy.

    Maybe it is the way to measure.

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.