Skip to main content
AVM
Associate II
Feb 10, 2022 5:31 AM UTC
Solved

How to read the reset cause using MC_RGM register on SPC58NG84E7 controller?

Hello,

I am currently working on SPC58NG84E7 controller with SPC5 studio.

I want to read the cause of reset in main routine.

In the reference manual, it is mentioned RGM register (RGM.FES & RGM.DES), which will help the controller to identify the type of reset.

I tried to read the RGM register in the beginning of my main function, but every time I am getting 0. I observed during debugging that, before entering into main routine, these registers are getting cleared. So, how to get the reset cause in main routine?

Regards,

AVM

    This topic has been closed for replies.
    Giuseppe DI-GIORE
    ST Employee
    Feb 27, 2022 10:28 PM UTC

    Hello,

    if you are using SPC5Studio, take into account that RGM.FES and RGM.DES are cleared, by software, at boot time.

    See file clock.c and function spc_clear_fccu_rgm(void)

    So, RGM.FES and RGM.DES registers are cleared by software.

    Modify clock.c to avoid to clear RGM FES and DES registers.

    Regards,

    2 replies

    Giuseppe DI-GIORE
    ST Employee
    Feb 27, 2022 10:28 PM UTC

    Hello,

    if you are using SPC5Studio, take into account that RGM.FES and RGM.DES are cleared, by software, at boot time.

    See file clock.c and function spc_clear_fccu_rgm(void)

    So, RGM.FES and RGM.DES registers are cleared by software.

    Modify clock.c to avoid to clear RGM FES and DES registers.

    Regards,

    bin zhuo
    Associate
    Mar 25, 2022 3:00 AM UTC

    Dear ST,

    I am also developing the FCCU function by SPC58EC80. I can read the reset cause by RGM.FES as FCCU(MCU_FCCU_HARD_RESET or MCU_FCCU_SOFT_RESET), but my goal is to read which fault channel source of FCCU caused the reset. So far, I haven't been able to achieve my goal.

    my step is read register RF_S and N2FF_STATUS of FCCU at main function startup, just like this:

    	FCCU.CTRL.R = FCCU_OP10;
    	while (FCCU.CTRL.B.OPS != 0x3) //0b:11 Successful
    	{
    		asm("nop");
    	};
    	FCCU_Log->RF_S0 = FCCU.RF_S[0].R;
    	FCCU_Log->RF_S1 = FCCU.RF_S[1].R;
    	FCCU_Log->RF_S2 = FCCU.RF_S[2].R;
    	FCCU_Log->RF_S3 = FCCU.RF_S[3].R;
     
    	FCCU.CTRL.R = FCCU_OP6;
    	while (FCCU.CTRL.B.OPS != 0x3) //0b:11 Successful
    	{
    		asm("nop");
    	};
    	FCCU_Log->N2FF_STATUS = FCCU.N2FF_STATUS.R;

    ​

    i use debugger mode and set breakpoint at this, when reset by FCCU(such as channel #8 reset reaction), the register RF_S and N2FF_STATUS always 0,just like this:

    0693W00000Lvh8BQAR.pngbecase i use channe #8 as the test, so i think RF_S0 should be 256. The facts did not meet expectations。

    Please help me,thanks !