Skip to main content
Erwan YVIN
ST Technical Moderator
Mar 25, 2024 9:45 AM UTC
StickySolved

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed 

It is typical IT Issue :face_screaming_in_fear:  in each corporate company.

“"Path building" refers to the process of verifying a chain of certificates from a specific certificate up to a root CA (Certificate Authority) certificate. If this process fails, it means that the application could not construct a trusted path from the server's certificate to a root CA.”

 

IMPORTANT : The customer needs to install their own root certificate in JRE StellarStudio keystore

  • Typically this keystore is at c:\StellarStudio-5.0\eclipse\jre\\lib\security\cacerts.

The keytool that is used to access the keystore is typically installed with the JRE and ready to use.

 

  • Run the standard keytool to import the certificate, from c:\StellarStudio-5.0\eclipse\jre\\lib\security\cacerts.

c:\StellarStudio-5.0\eclipse\jre\bin\keytool -import -trustcacerts -alias myrootCA -file myrootCA.cer -keystore cacerts

  • When prompted Enter keystore password:, enter "changeit".

By default keystores have a password of "changeit"

  • When prompted Trust this certificate? [no]:, enter "yes".

This imports the certificate into the keystore and display the message: "Certificate was added to keystore".

 

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Feb 7, 2025 10:02 AM UTC

Hello ,

Do not forget to update the cacerts in case of 

sun.security.validator.ValidatorException: PKIX path building failed 

c:\StellarStudio-7.1\eclipse\jre\bin\keytool -import -trustcacerts -alias myrootCA -file myrootCA.cer -keystore cacerts

            Best Regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINAuthorBest answer
ST Technical Moderator
Feb 7, 2025 10:02 AM UTC

Hello ,

Do not forget to update the cacerts in case of 

sun.security.validator.ValidatorException: PKIX path building failed 

c:\StellarStudio-7.1\eclipse\jre\bin\keytool -import -trustcacerts -alias myrootCA -file myrootCA.cer -keystore cacerts

            Best Regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.