Skip to main content
prashanth.mohan22
Associate III
May 24, 2019 11:46 AM UTC
Question

How to implement CAN TP for SPC560B series microcontroller?

Hi,

I need to serial transmit continuous stream of data via CAN. For that, is there any supported or modules already implemented to address CAN TP?

Your response shall be highly appreciated.

Regards,

Prashanth Mohan

    This topic has been closed for replies.

    7 replies

    Erwan YVIN
    ST Technical Moderator
    Jul 4, 2019 2:02 PM UTC

    Hello Mohan ,

    we have some example in the application available in SPC5Studio Tools Suite (CAN driver) is available

    SPC560Bxx_RLA CAN Test Application for Discovery

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    prashanth.mohan22
    Associate III
    Jul 5, 2019 6:47 AM UTC

    Hello Erwan,

    Thanks for your suggestion, but SPC560Bxx_RLA CAN Test Application for Discovery covers only examples for data transmission of 8 bytes. For more than 8 bytes, in case of flashing through CAN being in-compliance with UDS protocol, we require flow control to be implemented on the CAN driver.

    Please refer http://www.piembsystech.com/protocol/automotive-protocols/can-tp-protocol/ and suggest me on the same.

    Best regards

    Prashanth

    Explorer
    Nov 27, 2023 7:23 PM UTC

    I had the same issue and i personally requested the owner of PiEmbSysTech and they supported me on this. Its not only about the CAN-TP, if you have any doubts on any Embedded Systems or VLSI Related topics, you can send them mail for a support, they will support you, he is a nice guy and very talented and having knowledge from end to end from wherever you ask any questions. He is more sound in Bootloader or any Embedded & VLSI Core Topics with all the Embedded Protocols. In single word, I can say that he is the expert Scientist from hardware to software. 

    gp73
    Associate III
    Jul 8, 2019 8:39 AM UTC

    Hello,

    in my opinion you have to implement a TP by yourself, or you can buy it (there are some company that sell can driver + TP + UDS but is expensive).

    Otherwise you have to follow the requirements:

    ISO 14229-1 for UDS and ISO 15765-2, ISO 15765-2 for TP.

    Personally my view of these part of Sw are:

    can driver at driver layer that let you to receive and transmit maximum of 8 bytes

    tp at presentation layer that let you to receive and transmit a maximum of 4096 bytes (if I remember well) managing all the tipes of frame FF, FC,etc

    and UDS layer that let you to manage the UDS services and that is called from UDS.

    Hope this can be useful

    BEst regards

    prashanth.mohan22
    Associate III
    Jul 8, 2019 1:08 PM UTC

    Hi gp73,

    Very thanks for providing insight on this subject.

    Actually, I'm planning to implement TP on my own.

    Do you have any resources/support documents/ implementation guidelines that could help me to proceed further?

    I would be grateful for your suggestion.

    Thanks.

    Prashanth

    gp73
    Associate III
    Jul 8, 2019 2:12 PM UTC

    Unfortunately I can't share because these are owned by my previous company.

    But regarding the ISO you can buy and aren't expensive.

    prashanth.mohan22
    Associate III
    Jul 9, 2019 6:31 AM UTC

    Thank you so much gp73.

    @Erwan YVIN​ , Can you help me with support documents/design guidelines for implementing CAN TP with UDS?

    Regards,

    Prashanth