Skip to main content
PSing.5
Associate II
Jul 22, 2021 10:20 PM UTC
Solved

How to get double wire CAN from SPC5?

SPC5Studio asks for a TX and RX pin. I selected CAN 1 TX and RX pins and connected them to CAN 2 RX and TX pins I chose (I tried all manner of connections). I am trying to get CAN 2 to send a message. On the output I see a 0 to 5 V signal instead of 0 to 2.5 V and another of 2.5 to 5 V. How do I get two wire CAN? I think I am missing a concept here, can someone please help me.

I am trying to use SPC560B discovery board.

    This topic has been closed for replies.
    PSing.5
    PSing.5Best answer
    Associate II
    Jul 23, 2021 2:25 AM UTC

    To anyone reading this in the future, the answer to my question was the SPC56 DIS board does not come with a transceiver to produce a CAN_H and CAN_L.

    1 reply

    PSing.5
    PSing.5AuthorBest answer
    Associate II
    Jul 23, 2021 2:25 AM UTC

    To anyone reading this in the future, the answer to my question was the SPC56 DIS board does not come with a transceiver to produce a CAN_H and CAN_L.