Skip to main content
arro239
Associate III
Jul 30, 2014 2:54 AM UTC
Question

how to flash binary into spc563M-disp board?

Posted on July 30, 2014 at 04:54

I've compiled some code & I have .bin/.dmp/.elf/.hex/.map files.

How do I program/flash whichever I need to flash into spc563M-disp board? I do have a PLS device, the driver and UDE Desktop installed.

While AN4425 promises ''The document UM1602 (see Reference documents) is focused to describe and to understand how to use SPC5studio and how to create, build and debug a project.'', I do not see the word ''debug'' mentioned in UM1602 SPC5 Studio users guide even once, but maybe I am doing something wrong.

Please advice.
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    Jul 30, 2014 8:23 AM UTC
    Posted on July 30, 2014 at 10:23

    Hello Andrey ,

    To debug the project :

    1) Please check if the driver is well installed in DEVICE MANAGER (Cf screenshot)

    2) 2 possibilities : (cf screenshot)

    Example : on the repository

    you need to double-click on ''debug.wsx''

    or click on debug button on Activity wizard

    In your custom application you need to create a UDE directory like the test applications repository.

    With UDE , you will be able to flash and debug.

    Best Regards

    Erwan

    ________________

    Attachments :

    2014-07-30_091154.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWH2&d=%2Fa%2F0X0000000bo9%2F4xSBxVWULZT8iLmFaSrKHOoguB7Ems__jXSy2Xn4ziE&asPdf=false

    2014-07-30_101727.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qXcL&d=%2Fa%2F0X0000000bos%2FyHHOwtaAmwlkjXv_YRILV653IIwJZRvLjIVy4X3NvMo&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.