Skip to main content
rpoon
Associate II
Mar 17, 2020 11:53 AM UTC
Solved

How to check whether the SPC560B54L5 EVB IS IN STANDBY mode or not?

0693W000000U6AvQAK.jpgHello,

I am trying to make SPC560B54L5 EVB in low power mode that is STANDBY mode.

The measured current in normal RUN0 mode is 143 mA whereas while keeping in STANDBY mode, it is around 92 mA. But as per the AN3316 Application note the max current consumption is 314uA. So am I entering into STANDBY mode correctly?

Because I could see that USB is getting disconnected during waiting for the S_MTRANS to SET.

 while (ME.IS.R == 0U){

  ;

 }

How can I make sure rather SPC560B54L5 EVB is in standby mode or not?

BEST REGARDS

Rewatee

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Mar 17, 2020 2:40 PM UTC

    Hello Rewatee ,

    Maybe you have some measurement issues

    I am not an expert to measure a MCU in low power mode

    There is a nice example in the application wizard

    SPC560Dxx_RLA WKPU API Test Application for Discovery

    The core should display Core Inactive on a debug session

    Best Regards

    Erwan

    0693W000000U7QBQA0.png

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Mar 17, 2020 2:40 PM UTC

    Hello Rewatee ,

    Maybe you have some measurement issues

    I am not an expert to measure a MCU in low power mode

    There is a nice example in the application wizard

    SPC560Dxx_RLA WKPU API Test Application for Discovery

    The core should display Core Inactive on a debug session

    Best Regards

    Erwan

    0693W000000U7QBQA0.png

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.