Skip to main content
SLEE.6
Associate II
Nov 6, 2020 7:54 AM UTC
Solved

How to add PWM control in SPC58EC-DISP using Ethernet gateway

Hello!​

I have a SPC58EC-DISP and imported a sample application: Network Gateway Test; I added PWM control, but it keeps running PWM and cannot run the network gateway, what should I do? it used FreeRTOS.

 
/* eMIOS1 CH22 (PWM, GROUP2) period callback.*/
void emios1_gr2ch22_pcb(PWMDriver *pwmp) {
 
 (void)pwmp;
}
 
/* eMIOS1 CH22 (PWM, GROUP2) period callback.*/
void emios1_gr2ch22_cb(PWMDriver *pwmp) {
 
 (void)pwmp;
}
 
portTASK_FUNCTION(motorPwmTask, pvParam ) {
 (void)pvParam;
 
 
 pwm_lld_start(&PWMD14,&pwm_config_e1_gr2_pwmcfg);
 
 for( ; ; ){
 
 pwm_lld_enable_channel(&PWMD14, 5, PWM_PERCENTAGE_TO_WIDTH(&PWMD14, 5000), 100, 0, 0);
 
 }
 
}
 
uint32_t motor_pwm_start(void) {
 
 uint32_t ret;
 
 /* create motor pwm task */
 ret = xTaskCreate(motorPwmTask, "motorPwmTask", 1024, NULL, 6, NULL);
 
 return (ret == pdPASS) ? 0 : 1;
}
 
 
 
/*
 * Application entry point.
 */
int main(void) {
 
 uint32_t error;
 
 /* Initialization of all the imported components in the order specified in
 the application wizard. The function is generated automatically.*/
 componentsInit();
 
 /* Enable Interrupts */
 irqIsrEnable();
 
 encoder_setup();
 
 /* Start the motor pwm task */
 error = motor_pwm_start();
 
 /* Start the gateway task */
 error = gateway_start();
 
 if (!error) {
 /* Start the remote device emulation task */
 error = remote_start();
 }
 
 if (!error) {
 /* Start all tasks */
 vTaskStartScheduler();
 }
 
 /* If all is well, the scheduler will now be running, and the following
 line will never be reached. If the following line does execute, then
 there was insufficient FreeRTOS heap memory available for the idle and/or
 timer tasks to be created. See the memory management section on the
 FreeRTOS web site for more details. http://www.freertos.org/a00111.html */
 for( ;; ) {}
 
 return 0;
}
 

    This topic has been closed for replies.
    Piranha
    PiranhaBest answer
    Principal III
    Nov 6, 2020 7:58 PM UTC

    The pwm_lld_enable_channel() is called non-stop and therefore none of lower priority tasks don't get CPU time. As a quick workaround add some delay with vTaskDelay() after that call.

    3 replies

    Piranha
    PiranhaBest answer
    Principal III
    Nov 6, 2020 7:58 PM UTC

    The pwm_lld_enable_channel() is called non-stop and therefore none of lower priority tasks don't get CPU time. As a quick workaround add some delay with vTaskDelay() after that call.

    SLEE.6
    SLEE.6Author
    Associate II
    Nov 10, 2020 2:44 AM UTC

    Thank you for your help,It's working.

    Giuseppe DI-GIORE
    ST Employee
    Nov 13, 2020 3:05 PM UTC

    Hello,

    no need to run pwm_lld_enable_channel() in a loop.

    Call it once and the eMIOS will keep PWM going on.

    Call other PWM driver functions to change period and/or duty (not in a loop).

    Regards,

    Giuseppe