Skip to main content
Catalin
Visitor II
Oct 17, 2018 9:14 AM UTC
Question

How do I proceed a wakeup on SPC584Cx/SPC58ECx 32-bit MCU Chorus 4M?

Hello everybody,

My name is Catalin and I work on an Automotive project on a gateway and I have a question regarding this microcontroler.

So basically I have to wakeup the gateway every 600 seconds +/- 15 seconds and perform a voltage measurement. As I read in the reference manual there is this RTC_APIVAL register which its bits are compared to the RTC counter bits and if a match occurs, an wakeup request is asserted. I tried in so many ways to make that work but I didn't manage to do it.

Here is my code so far:

void rtc_init(void)
{
	/*Disable Real Timer Counter Module for initialization*/
	RTC_API.RTCC.B.CNTEN = 0u;
 
	PMCDIG.MISC_CTRL_REG.B.SIRC_ENB = 0; // Enable SIRC in running modes
	RC128K_DIG.CTL.B.LPRCON_STDBY = 1; // Enable SIRC in STANDBY
 
	/*select clock SIRC 128 KHz*/
	RTC_API.RTCC.B.CLKSEL = 1u;
	/*enable divider by 32*/
	RTC_API.RTCC.B.DIV32EN = 1u;
	/*disable divider by 512*/
	RTC_API.RTCC.B.DIV512EN = 0u;
 
	RTC_API.RTCC.B.APIEN = 0;
	RTC_API.RTC_APIVAL.B.APIVAL = 2400000; // API period 1/4000Hz * 2400000= 600sec?
	RTC_API.RTCC.R = 0x80009001; //Counter enabled, API enabled, SIRC@128KHz used, Trigger enabled for Analog Comparator Block
}

And this is how I call it:

{ 
...
	WKPU.WISR.R = 0x0002u; // clear possible RTC
	rtc_init();
	RTC_API.RTCS.R = 0x200002400; // Clear RTC flags
 
...
}

Can you have a look at this code? It doesn't seem to work but I build it based on the reference manual.

Maybe the value of the APIVAL(2400000) is not good(It's not 600 seconds)?

Thank you. Best regards,

Catalin

This topic has been closed for replies.