Skip to main content
Nicola Bogoni
Visitor II
Jun 23, 2017 12:03 PM UTC
Solved

How create section in SPC5 studio?

Posted on June 23, 2017 at 14:03

Hi everybody,

I'm using SPC560P50L5 processor.

I need to declare some sram program and data sections. How can i do in spc5 studio?

my code consist in different function, and each of this need a particoulare storage address zone and a particoular ram zone.

Are there the possibility to create a personal application.id file?

Are there a possibility to do that outside application.id file (for example into main.c file)?

Thank you very much

Nicola

#spc5 #memory-sections-ram-linker #memory-sections
    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 23, 2017 1:44 PM UTC
    Posted on June 23, 2017 at 15:44

    Hello ,

     yes , you can create your own linker file

    you can declare your section in user.ld

    1) Copy-paster Application.ld file

    2) rename it by user.ld

    3) add your sram section

                Best regards

                                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jun 23, 2017 1:44 PM UTC
    Posted on June 23, 2017 at 15:44

    Hello ,

     yes , you can create your own linker file

    you can declare your section in user.ld

    1) Copy-paster Application.ld file

    2) rename it by user.ld

    3) add your sram section

                Best regards

                                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    PGaik
    Associate
    Jun 27, 2019 9:37 AM UTC

    i can able to create the my own user.ld file with different flash memory section (i.e. Calibration, bootloader and application).

    Now what happen whenever i am doing the clean the project and regenerate the SPC driver then automatically IDE generate the default application.ld file. So, is there any setting which can tell the IDE and compiler that mot to generate the default application. ld linker file