Skip to main content
BCHOI.1
Visitor II
Nov 16, 2021 2:03 PM UTC
Solved

How can I use LIN Slave mode? (SPC58EC-Disp)

Hi, I want to use LIN communication as slave in my board.

I'm using SPC5Studio, and I'm checking the example code which the SPC58ECxx_RLA LIN Test Application for Discovery.

This example code is used two LIN nodes and master node ask for data to slave node. (202 code line)

I have expect when slave node receive ask something from the master node, this program access spc5xx_lin_rxi_interrupt API.

But If I use just only slave node, How Can I use transmit function?

I think one of solution is modification of spc5xx_lin_rxi_interrupt API, but is it have another solution?

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 18, 2021 4:03 PM UTC

    Hello ,

    The slave setting is in synchronous mode.

    read/write function will block until operation has been completed

    you do not need to update spc5xx_lin_rxi_interrupt_api

    you can use the callback slave_tx_callback or slave_rx_callback

    0693W00000GY4EnQAL.png 

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Nov 18, 2021 4:03 PM UTC

    Hello ,

    The slave setting is in synchronous mode.

    read/write function will block until operation has been completed

    you do not need to update spc5xx_lin_rxi_interrupt_api

    you can use the callback slave_tx_callback or slave_rx_callback

    0693W00000GY4EnQAL.png 

    Best regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.