Skip to main content
BKIM.11
Visitor II
Apr 28, 2020 9:18 AM UTC
Solved

how can i programming uart interrupt(sd_lld_read)?

hello,

I am using the SPC582b and SPC5stdio.

I want to have interrupts run whenever I receive data.

But This function is difficult because it waits until input is received

(sd_lld_read, &lcd_data[bit], 1)

How can I implement an uart interrupt?

I need your help.

Thank you.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    May 4, 2020 12:45 PM UTC

    Hello ,

    You can use a thread by using a RTOS like Chibios or FreeRTOS

    or you can adapt the driver presents in this followin g file

    **
     * @brief Serial read without DMA
     *
     * @param[in] sdp pointer to a @p SerialDriver object
     * @param[out] buffer data buffer receiver
     * @param[out] len number of bytes received
     *
     * @return The number of bytes effectively read.
     *
     * @notapi
     */
    static uint16_t sd_rx(SerialDriver* sdp, uint8_t* buffer, uint16_t len) {
     
     if (len > 0UL) {
     if(sdp->config->api_mode == SPC5_LIN_API_MODE_BUFFERED_IO) {
     uint16_t l = len;
     sdp->linflexlp->LINIER.B.DRIE = 0;
     while (l != 0U) {
     if (sdp->rx_read_ptr != sdp->rx_write_ptr) {
     sdp->linflexlp->LINIER.B.DRIE = 0;
     *buffer++ = *sdp->rx_read_ptr++;
     if (sdp->rx_read_ptr == sdp->rx_end_ptr) {
     sdp->rx_read_ptr = sdp->rx_buffered_io;
     }
     l--;
     } else {
     sdp->linflexlp->LINIER.B.DRIE = 1;
     }
     }
     sdp->linflexlp->LINIER.B.DRIE = 1;
     } else {
     sdp->rx_buf = buffer;
     sdp->rx_len = len;
     sdp->linflexlp->LINIER.R |= (uint16_t)(SPC5_LINIER_DRIE | SPC5_LIN_INTERRUPTS); /* Interrupts enabled. */
     sdp->linflexlp->UARTCR.B.RXEN = 1;
     }
     }
     return len;
    }

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    May 4, 2020 12:45 PM UTC

    Hello ,

    You can use a thread by using a RTOS like Chibios or FreeRTOS

    or you can adapt the driver presents in this followin g file

    **
     * @brief Serial read without DMA
     *
     * @param[in] sdp pointer to a @p SerialDriver object
     * @param[out] buffer data buffer receiver
     * @param[out] len number of bytes received
     *
     * @return The number of bytes effectively read.
     *
     * @notapi
     */
    static uint16_t sd_rx(SerialDriver* sdp, uint8_t* buffer, uint16_t len) {
     
     if (len > 0UL) {
     if(sdp->config->api_mode == SPC5_LIN_API_MODE_BUFFERED_IO) {
     uint16_t l = len;
     sdp->linflexlp->LINIER.B.DRIE = 0;
     while (l != 0U) {
     if (sdp->rx_read_ptr != sdp->rx_write_ptr) {
     sdp->linflexlp->LINIER.B.DRIE = 0;
     *buffer++ = *sdp->rx_read_ptr++;
     if (sdp->rx_read_ptr == sdp->rx_end_ptr) {
     sdp->rx_read_ptr = sdp->rx_buffered_io;
     }
     l--;
     } else {
     sdp->linflexlp->LINIER.B.DRIE = 1;
     }
     }
     sdp->linflexlp->LINIER.B.DRIE = 1;
     } else {
     sdp->rx_buf = buffer;
     sdp->rx_len = len;
     sdp->linflexlp->LINIER.R |= (uint16_t)(SPC5_LINIER_DRIE | SPC5_LIN_INTERRUPTS); /* Interrupts enabled. */
     sdp->linflexlp->UARTCR.B.RXEN = 1;
     }
     }
     return len;
    }

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.