Skip to main content
MRama.11
Visitor II
Sep 18, 2020 8:47 AM UTC
Solved

how can i log data to SDcard using SPI in SPC58EC-Disp

I have an SPI SD Card interface how can i log to my memory card using this module and Free RTOS+FATFS module .

Please provide some examples program if possibles or other alternate solutions

This topic has been closed for replies.
Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Sep 23, 2020 8:08 AM UTC

Hello ,

the good example on SPC58 Family with FreeRTOS+FATFS is in the application :

SPC58xGxx_RLA HTML FTP CLI Test Application for Discovery

I recommend to analyze this application (Pinmap and configuration) and port it for SPC58EC for FreeRTOS-FAT

There are others applications using SPI Transfer for SPC58EC.

I recommend to mix them.

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
Sep 23, 2020 8:08 AM UTC

Hello ,

the good example on SPC58 Family with FreeRTOS+FATFS is in the application :

SPC58xGxx_RLA HTML FTP CLI Test Application for Discovery

I recommend to analyze this application (Pinmap and configuration) and port it for SPC58EC for FreeRTOS-FAT

There are others applications using SPI Transfer for SPC58EC.

I recommend to mix them.

Best Regards

Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.