Skip to main content
Lde.815
Associate II
May 6, 2020 3:39 AM UTC
Question

Hi, Hi, My setup: SPC560Pxx_RLA SWT Test Application for Discovery uC: SPC560P50L3 IDE: SPC5Studio 5.8.1 This problem occurs when emulator links. Tu 21.04.2020 16:07:54.541, Error, Core::PowerPcInstr, could not access 0x00000000

Our program can run when connected to the debugger, but it can't run automatically when unplugged and recharged. What's the problem?

    This topic has been closed for replies.

    5 replies

    Erwan YVIN
    ST Technical Moderator
    May 7, 2020 8:26 AM UTC

    Hello ,

    Do you use PLS Debugger or TRACE32 debugger ?

    have you flashed your software ?

    Could you check your jumpers ?

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Lde.815
    Lde.815Author
    Associate II
    May 7, 2020 9:11 AM UTC

    Thank you!

    • The board I used was designed by myself, and there is no problem with the reset electricity.
    • The emulator I use is spc5-udestk-eval.
    • To make sure my program is working properly.
    • An error occurs whenever the emulator links to the board.
    •  

    Kind regards

    0693W000000X3EWQA0.png

    Lde.815
    Lde.815Author
    Associate II
    May 7, 2020 9:08 AM UTC

    Thank you!

    Giuseppe DI-GIORE
    ST Employee
    May 8, 2020 10:18 AM UTC

    It is a matter of emulator configuration. Check the configuration files.

    Lde.815
    Lde.815Author
    Associate II
    May 9, 2020 2:26 AM UTC

    Thank you�?

    • Since it is not clear for me to use it for the first time, could you please tell me how to configure it in detail?Or do you have any recommendations?
    •  
    • As shown below, what is the reason for this?(i.e. Error, Core::PowerPcInstr, could not access 0x00000000)0693W000000X3EWQA0.png

    Kind regards