Skip to main content
Ravi S
Associate II
Mar 10, 2022 12:07 PM UTC
Question

Hi Guys, I am working on SPC584B-DISP Board.In this board i need bootloader option so that i am try to use example SPC584Bxx_RLA Bootloader Test Application for Discovery 2 .In this example download code from serial UART .

In this I can able to download bin file from UART next step jump to app in this step not working if any one have idea please help .......

Thanks advance ...

    This topic has been closed for replies.

    52 replies

    ODOUV.1
    ST Employee
    Mar 11, 2022 9:54 AM UTC

    Hello,

    I suppose you want to flash your program via USB/uart

    Then you need to configure the connection in SERIAL instead of CAN

    and use peripheral LINFLEX_4 at 1152000693W00000KcED5QAN.pngThen in the PINMAP wizard, you have to configure the PIN 113 (port PA[0]) in input LIN4_RXD0693W00000KcEFBQA3.png 

    On PC tool side, also use 115200 baud rate

    Best regard,

    -Olivier

    ODOUV.1
    ST Employee
    Mar 14, 2022 7:52 AM UTC

    Hello,

    it also needs to configure pin 114 in with LIN4_TX because the embedded firmware updater must answer to PC flash loader:0693W00000KcSrsQAF.pngBest regards,

    -Olivier

    Ravi S
    Ravi SAuthor
    Associate II
    Mar 15, 2022 9:58 AM UTC

    Hi sir ,

    Thanks for your replay

    Sorry for the late reply

    I already dune everything above you mentioned but code not jump to latest code .see my configuration on below screenshot

    0693W00000KceARQAZ.png0693W00000KceAgQAJ.png0693W00000KceAlQAJ.png

    Ravi S
    Ravi SAuthor
    Associate II
    Mar 15, 2022 10:12 AM UTC

    Hi sir,

    Currently I am facing two problems.

    Problem 1:-

    First I loaded bootloader code into debug mode (Load to RAM -0x00FC0000).

    Put the breakpoint to SPC5_UPDATER_IDLE,SPC5_UPDATER_GETSIZE,SPC5_UPDATER_GETDATA.

    send the password ,size ,bin file from other controller I can able to write all bin file into 0x01000000 location .

    Then while debug I restart the code and I put the breakpoint into inside updater_jump() function .pointer coming to inside the jump to function but new code not executed.

    Problem 2:-

    I loaded bootloader code into flash (Execute from Flash -0x00FC0000).

    Run the code first step I send password from other controller I got response from SPC 5 MCU.

    Then I send Size from other controller I am not getting any response from SPC5.

    I fount issue with flasherase function.In this function working fine while debug mode but run from flash code stuck into this flasherase function .

    I attached screenshot for your reference

    0693W00000KceN1QAJ.pngyou have any idea pls let me know.

    Thanks regards

    Ravi.S

    .

    ODOUV.1
    ST Employee
    Mar 15, 2022 10:13 AM UTC

    Hello,

    on your first image, I recommend to choose a timout of 5000 ms

    on your second image, choose LINFLEX_4

    on your third image, configure pin 113 and pin 114 on LINFLEX_4

    Best regards,

    -Olivier

    Ravi S
    Ravi SAuthor
    Associate II
    Mar 15, 2022 10:18 AM UTC

    Hi sir

    on your first image, I recommend to choose a timout of 5000 ms

    That also I tried I am facing same issue.Ok I will change.

    on your second image, choose LINFLEX_4

    If I use LINFLEX_6 it make any problem sir.

    on your third image, configure pin 113 and pin 114 on LINFLEX_4

    LINFLEX_6 make any problem tell me sir then i will change to this pin .

    Thanks regards

    Ravi.S

    ODOUV.1
    ST Employee
    Mar 15, 2022 10:24 AM UTC

    There is no issue with LINFLEX_6,

    but the UART/USB is connected on LINFLEX_4 on this board:0693W00000KceW8QAJ.pngso if you want to flash with USB, you need to use LINFLEX_4

    BRs,

    -Olivier

    Ravi S
    Ravi SAuthor
    Associate II
    Mar 15, 2022 10:41 AM UTC

    HI sir

    Thanks for your replay .

    I want to flash code from other controller via UART .If I connected LINFLEX_6 to my other controller then my setting is Ok right . I attached the picture for your reference.

    0693W00000KceiOQAR.jpgMy aim is

    I want to upload spc584b-disp board via Uart from other MCU .

    Thanks regards

    Ravi.S

    ODOUV.1
    ST Employee
    Mar 15, 2022 10:53 AM UTC

    I got it,

    you don't use PC tool connected to USB, but another MCU is connected to LINFLEX6 in serial mode to flash the SPC584B.

    Thanks,

    I will forward your question to a bootloader/flash expert.

    BRs,

    -Olivier

    Ravi S
    Ravi SAuthor
    Associate II
    Mar 15, 2022 11:08 AM UTC

    Yes sir. I want to flash the SPC584B from other MCU(STM32 ) via UART

    I explain one more time .

    I have two MCU One is SPC584b-Disp board other one is STM32 or some other MCU.

    I what to send bin file from STM32 to SPC584B-Disp via UART if i have any update .SPC584B-Disp board need bootloader code after restart wait for 5 s that time if any code available send the new .bin file from STM32 to SPC5 board via UART. Bootloader need to write code into the flash once completed jump to new code this is i want sir .

    That's why i try to use SPC584Bxx_RLA Bootloader Test Application for Discovery 2 example code for my application I am facing above mention issue.

    Pls try to give some idea to solve this issue .

    Thanks regards

    Ravi.S