Skip to main content
Logeshwar
Associate
Jul 5, 2022 5:47 AM UTC
Solved

Hey all I have a problem with SPC56ECxx. The question is I have to create a single program for both the cores (core 1 : z4d and core 2 : z0h) or I have to create a separate program for z4d and z0h. If I need to create separate program for z4d and z0h

How to debug those separated code via winIDEA.

    This topic has been closed for replies.
    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 5, 2022 9:00 AM UTC

    Hello ,

    Winidea seams to support SPC56 Families.

    I recommend to create a separate program for z4d and z0h

    you have an example on http://community.spc5studio.com (HAL Components Update Site)

    SPC56ECxx OS-Less Z0 Slave Core Test Application

    SPC56ECxx OS-Less Z4 Master Core Test Application

    For this case , we have created 2 applications.

    You can create with the same spirit 2 RLA applications (z4d and z0h)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

    5 replies

    ODOUV.1
    ST Employee
    Jul 5, 2022 8:35 AM UTC

    Multicore debugging is supported by UDE/PLS, our partner

    If you are using WINIDEA, contact them to know if they are supporting SPC5xx multicore debugging.

    Best regards

    Logeshwar
    LogeshwarAuthor
    Associate
    Jul 5, 2022 8:46 AM UTC

    I have to create a single program for both the cores (core 1 : z4d and core 2 : z0h) or I have to create a separate program for z4d and z0h. Can you answer this?

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    Jul 5, 2022 9:00 AM UTC

    Hello ,

    Winidea seams to support SPC56 Families.

    I recommend to create a separate program for z4d and z0h

    you have an example on http://community.spc5studio.com (HAL Components Update Site)

    SPC56ECxx OS-Less Z0 Slave Core Test Application

    SPC56ECxx OS-Less Z4 Master Core Test Application

    For this case , we have created 2 applications.

    You can create with the same spirit 2 RLA applications (z4d and z0h)

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Logeshwar
    LogeshwarAuthor
    Associate
    Jul 5, 2022 9:18 AM UTC

    Thank you sir. I have one more doubt If i create separate program, Then how can I able to communicate the cores with each other

    Sivashankar
    Associate II
    Jul 6, 2022 6:01 AM UTC

    I couldnt get the sample codes for sample Slave core and Master core Test Application. Please guide me to get those codes. That website is not working...