Skip to main content
ivancolla9
Associate III
Jan 29, 2016 3:16 PM UTC
Solved

Help using the ADC

Posted on January 29, 2016 at 16:16

Good morning,

I am trying to activate and use tha A/D converter. After activating the peripheral, I proceed to set the register in this way:

ADC0.NCMR0.R = 0b00000000000000001111111111111111; /* Enable all conversion channel for test.*/
ULONG OWREN_MASK = 1 << 31; /* Enable conversion data to be overwritten. */
ULONG WLSIDE_MASK = 1 << 30; /* Conversion data written right-aligned. */
ULONG MODE_MASK = 1 << 29; /* Continuous scan conversion. */
ULONG START_MASK = 1 << 24; /* Start conversion on enabled channels. */
ADC0.MCR.R = OWREN_MASK | WLSIDE_MASK | MODE_MASK | START_MASK;

when I execute the code on the discovery board, I wait for a valid data on one of the channels.

if (ADC0.CDR0.B.VALID == 1)

Following discovery-board manual, the AD0 port (B7), is accessible via pin A26 of the connector. I connect to that pin a 5 V voltage, expecting to read something. The problem is that I don't read anything. Monitoring the all the CDRn registers, I see that neither of them has a new convertion valued stored: tha data field is 0 and the VALID field is 0. What am I missing? Regards, Ivan #discovery #adc #board
This topic has been closed for replies.
ivancolla9
ivancolla9Best answer
Associate III
Feb 1, 2016 4:25 PM UTC
Posted on February 01, 2016 at 17:25

Hello Erwan,

I discovered the issue and it was more simple that I belevied. It was necessary separate the configuration registry input to the start register input. To be clear, I changed

ADC0.MCR.R = OWREN_MASK | WLSIDE_MASK | MODE_MASK | START_MASK;

with

ADC0.MCR.R = OWREN_MASK | WLSIDE_MASK | MODE_MASK;
ADC0.MCR.R = ADC0.MCR.R | START_MASK;

As you can see, first I configure the MCR registry, than I give the start settin to 1 the NSTART bit field (using the mask). Doing so, the channel configured are activated and I can read the input vlaue of the ADC. Regards, Ivan

2 replies

Erwan YVIN
ST Technical Moderator
Feb 1, 2016 2:42 PM UTC
Posted on February 01, 2016 at 15:42

Hello Ivan ,

Did you solve your issue ? you should receive EOC Interrupt (end Of Conversion)

IRQ_HANDLER(SPC5_ADC1_EOC_HANDLER) {

Best regards Erwan
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ivancolla9
ivancolla9AuthorBest answer
Associate III
Feb 1, 2016 4:25 PM UTC
Posted on February 01, 2016 at 17:25

Hello Erwan,

I discovered the issue and it was more simple that I belevied. It was necessary separate the configuration registry input to the start register input. To be clear, I changed

ADC0.MCR.R = OWREN_MASK | WLSIDE_MASK | MODE_MASK | START_MASK;

with

ADC0.MCR.R = OWREN_MASK | WLSIDE_MASK | MODE_MASK;
ADC0.MCR.R = ADC0.MCR.R | START_MASK;

As you can see, first I configure the MCR registry, than I give the start settin to 1 the NSTART bit field (using the mask). Doing so, the channel configured are activated and I can read the input vlaue of the ADC. Regards, Ivan