Skip to main content
Associate II
Jun 5, 2025 6:28 PM UTC
Question

Getting started with SPC560P-DISP

Just got an SPC560P-DISP and I'm following AN4487 Getting started instructions. I have the board connected via USB to my computer and I've got SPC5Studio up and running with a Serial Test App. I have cleaned, generated and compiled the app. Following along in the guide, opening the debug.wsx doesn't open a new window but rather the file itself in eclipse. The "Execute and debug your application" action is also grayed out. I've tried installing "udestk-5-02-04-spc5-stk" and CDM2123620 FTDI drivers.

After the "udestk-5-02-04-spc5-stk" was installed, in Device Manager, it went from a driverless device to PLS USB JTAG Adapter for SPC5xxx A/B. I've opened UDE STK independently of SPC5Studio and opened the debug.wsx file. This seems to allow me to flash a program to the board. I wanted to try and see if I could connect via Serial but there were no open COM ports from the device itself. After unplugging and plugging back in the board, it goes back to the LEDs blinking program the board came with. 

What am I missing here? Any help would be greatly appreciated. 

 

This topic has been closed for replies.