Skip to main content
dominik2
Associate II
May 19, 2015 11:28 AM UTC
Question

Generate Code with PinMap Wizard for Multi IDE Green Hill Compiler

Posted on May 19, 2015 at 13:28

I wonder if it is possible to generate C Code with the PinMap Wizard for use with the Multi IDE Green Hill Compiler and if that is possible how to integrate the code to a Multi IDE Project?

Thanks in advance,

Dominik
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    May 21, 2015 9:48 AM UTC
    Posted on May 21, 2015 at 11:48 Hello Dominik , Sorry for my late answer. I have never done this step. i think that it is possible. From SPC5Studio, you should reuse board.c / board.h generating from Pinmap Wizard after saving and generation from your configuration editor . and reimport the function in your greenhills application. the init is done by HAL :

    palInit(&pal_default_config);

    and

    /* Initial setup of all defined pads, the list is terminated by a {-1, 0, 0}.*/
    static
    const
    spc_siu_init_t spc_siu_init[] = {
    {PCR(PORT_A, PA_BUTTON), PAL_LOW, PAL_MODE_INPUT_PULLUP},
    {PCR(PORT_B, PB_LIN0_TDX), PAL_HIGH, PAL_MODE_OUTPUT_ALTERNATE(1)},
    {PCR(PORT_B, PB_LIN0_RDX), PAL_HIGH, PAL_MODE_INPUT},
    {PCR(PORT_A, PIN_GPIO2), PAL_LOW, PAL_MODE_INPUT},
    {PCR(PORT_B, PB_TRIMMER), PAL_LOW, PAL_MODE_INPUT_ANALOG},
    {PCR(PORT_A, PIN_GPIO3), PAL_HIGH, PAL_MODE_INPUT},
    {PCR(PORT_C, PC_LED8), PAL_LOW, PAL_MODE_OUTPUT_PUSHPULL},
    {PCR(PORT_C, PC_LED7), PAL_LOW, PAL_MODE_OUTPUT_PUSHPULL},
    {-1, 0, 0}
    };
    /* Initialization array for the PSMI registers.*/
    static
    const
    uint8_t spc_padsels_init[SPC5_SIUL_NUM_PADSELS] = {
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 0, 
    0, 0, 0, 0, 0, 0, 0, 
    };
    /**
    * @brief PAL setup.
    */
    const
    PALConfig pal_default_config = {
    PAL_MODE_UNCONNECTED,
    spc_siu_init,
    spc_padsels_init
    };

    Best Regards Erwan
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.