Skip to main content
Bruno Dalvit
Visitor II
Sep 27, 2017 10:03 AM UTC
Question

FPU exceptions on SPC56EL60L3

Posted on September 27, 2017 at 12:03

Hi all,

I'm developing on a SPC56EL60L3 device, using SPC5 Studio, I have two querstions about the FPU:

1. executing a division of a float number by 0.0F I would expect an infinite result (which means a 0bS111 1111 1xxx .... xxxx value, according with IEEE 754 standard), dividing 0.0F by 0.0F I would expect a NaN result (0bS111 1111 10xx ... xxxx value); in both cases the result is 0bS111 1111 0111 1111 .... 1111, which is a valid number (3.40...e+038).

Can you confirm that the SPC56 implements the IEEE 754 standard? What's wrong in my tests?

2. moreover I would expect the FPU to generate an exception (IVOR33), which is actually not managed by device. Can you please post a piece code explaining how to enable and manage that interrupt?

thanks in advance

best

Bruno

    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    Sep 28, 2017 9:12 AM UTC
    Posted on September 28, 2017 at 11:12

    Hello Bruno ,

    SPC56EL60 has 2 e200z4

    According to the e200z4 booke  e200z4 Power Architectureâ„¢ Core Reference Manual

    It seems to be compliant for IEEE 754, there is a FPU (Float process Unit)

    have you compiled with -mspe=yes ?

         Best regards

                  Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Erwan YVIN
    ST Technical Moderator
    Sep 29, 2017 9:24 AM UTC
    Posted on September 29, 2017 at 09:24

    Hello Bruno ,

    Did you enable the register 

    Signal Processing Extension/Embedded Floating-Point Status and

    Control Register (SPEFSCR)

    5

    (37)

    FDBZH Embedded Floating-point Divide by Zero High

    The FDBZH bit is set to 1 when a floating-point divide instruction executed with a high

    element divisor of 0, and the high element dividend is a finite non-zero number. FDBZH is

    cleared by a scalar floating point instruction. ?

             Best regards  

                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.