Skip to main content
aurelien23
Associate III
May 12, 2015 12:11 PM UTC
Question

FlexCAN filter duplicated on all configurations

Posted on May 12, 2015 at 14:11

Hello,

I'm using both FlexCAN of SPC56EL60 on SPC5 Studio 3.4.3 and I wanted to define filters for each of them. I created a config for each of them containing different filters. CAN1 has 16 filters from 0x200 to 0x20F and CAN2 has 16 filters from 0x400 to 0x40F.

--> 1st problem: all filters are merged in all config (CAN1 filters config was 0x200 to 0x20F AND 0x400 to 0x40F). I had to edit can_lld_cfg.c manually.

--> 2nd problem: the Rx mailbox number is fixed for both FlexCAN. The code generator does not allow to set a specific number for each FlexCAN.

--> 3rd problem: setting Rx mailbox number to 16 does not affect the function can_lld_is_rx_nonempty which only checks the first 8 mailboxes when not using the CAN_ANY_MAILBOX constant.
    This topic has been closed for replies.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    May 13, 2015 8:58 AM UTC
    Posted on May 13, 2015 at 10:58

    Hello Aurélien ,

    --> 1st problem: all filters are merged in all config (CAN1 filters config was 0x200 to 0x20F AND 0x400 to 0x40F). I had to edit can_lld_cfg.c manually.

     

    You are right ,

    it is a issue in CAN Layer (ftl file)

    we have submitted a ticket for this. (Error report)

    --> 2nd problem: the Rx mailbox number is fixed for both FlexCAN. The code generator does not allow to set a specific number for each FlexCAN.

     

    No , in this case .. it is not possible.

    It is a change request for this.

    --> 3rd problem: setting Rx mailbox number to 16 does not affect the function can_lld_is_rx_nonempty which only checks the first 8 mailboxes when not using the CAN_ANY_MAILBOX constant.

    Yes , it is another ER.

    As a temporary solution , you can patch the file in components/lib/src or include file.

    We will handle the ERs as soon as possible.

       Best regards

                   Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    aurelien23
    Associate III
    May 18, 2015 1:56 PM UTC
    Posted on May 18, 2015 at 15:56

    Regarding the 2nd problem, how could different FlexCANs could have a different number of Rx mailboxes since all CAN config definition are based on the CANConfig type which is using the unique CAN_RX_MAILBOXES size definition?

    Erwan YVIN
    ST Technical Moderator
    May 18, 2015 3:18 PM UTC
    Posted on May 18, 2015 at 17:18

    Yes , we have submitted in our database a change request  to have a different set of Rx Mailbox Number.

    Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.